In DDR3_design_sprabi1b, section 4.3.1.10, there is a minimum write leveling skew of 365 ps for DDR3-1333 in Table 18. This translates into about 2.03 inches of trace difference between the command line and data line. This is an awful long skew. Can some one enlighten me on this? If I only had one DDR3 memory chip, this requirement would mean I have to lengthen the data line by 2.03 in at least? This is hard to understand !