Other Parts Discussed in Thread: PMP
Hi:
I've flashed my u-boot.bin ,uImage,and rd-jffs2.bin into nand flash,
but there were some problems with the booting process,
could anyone help me out of these?
my console lags are as below:
U-Boot 2010.06 (Jan 30 2015 - 17:20:36)
TI8168-GP rev 2.1
ARM clk: 987MHz
DDR clk: 796MHz
I2C: ready
DRAM: 2 GiB
NAND: HW ECC BCH8 Selected
256 MiB
MMC: OMAP SD/MMC: 0
:,;;:;:;;;;;;;;r;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:;;;;;;;;:,;;:;:
;,;:::;;;;r;;;rssiSiS552X5252525259GX2X9hX9X9XX2325S55252i5:,;;:;:;;;;;;;;:,;;:
;:;;;;;;;rrssSsS52S22h52299GGAAMHMM#BBH#B#HMM#HMBA&&XX2255S2S5Si:,;;:;:;;;;;;;;
;:;;r;;rsrrriiXS5S329&A&MH#BMB#A&9XXA252GXiSXX39AAMMMBB&G22S5i2SSiiiisi:,;;:;:;
;;;;;r;rr2iisiih393HB#B#AA99i22irrrX3X52AGsisss2Xii2299HBMA&X2S5S5iSiisSsi:,;;:
r:r;rrsrsihXSi2&##MHB&Ahh3AGHGA9G9h&#H##@@@##MAMMXXX9SSS29&&HGGX2i5iisiiisisi:,
;;rrrrsSiiiA&ABH&A9GAGhAhBAMHA9HM@@@@@@@@@@@@@@@@@@@HHhAh2S2SX9&Gh22SSiisiiisii
r:rrssisiS2XM##&h3AGAX&3GG3Ssr5H@M#HM2; ;2X&&&MHMB###GBB#B&XXSSs529XX55iSsisisi
r;rsrisSi2XHAhX99A3XXG&&XS;:,rH#HGhAS @@@@3rs2XBM@@A552&&AHA2XiisSS252SSsisSs
r;issi5S22&&3iSSX292&hXsr;;:;h@&G339&S9@@@@2@MA&9&HB##Xris29ABMAAX2ir;rsSi5iss5
rrsSi2XhG&9GXh399&X99i;;;;;;r#H&293H9X#@@@@@@@B&9GhAH@XrrsrsiXABHB&HG2rr;rrSiSi
;:rsisS599&AA9XG&3A35r;:::;,;BMh&&2iX5A@@@@@@@&392X5GB2;;;r;iSX393A##A&Xi:::rsi
;:rss552222X553&XHMhir;;::,:,h#HhGSXhG3#@@@@#AXXS2XAHA;::;;;;ss55XShBA3239r:,;;
r;ii2S5SSi2i53hirsh2srr::,,,,;MMXX359&Ah3h&Si59SX99A#i:,::::;;sri2,.2r;:SGAr;,:
;:;rrrrssiriXGSi::shs;;;,,,:,,rBBA9h5s5h5iS5isi2SAHB5:,,,:::;rrs5&SrisSX5Srrr:,
;,r;;;;rsriSSrrrr;;5Xrr;;,:,,.,;9AA2SsisS5323XXXG9&i:.,,::;;r;;;srrrrrr;;:;::::
:,;r;r;rrissrrr;:;::;s;;;;,:,,..,r293h222hXXAAGGGX;:,,,:,:,::;:;::,:,,,,...,,,,
;,;;;;rrrrrrrrirr;,.,,:::::::,,,,.,;SX&ABAB2hhXir:,,.,,.,,:,,,,..,,,..,..,,,..:
:.:;:;;;:;;;;r;rrs;:.. ,,:::::,:,:,,.::rrsrr;;,,.......,..,....,,,,,,,...,.,,:,
:.:::,::::::;;r;rrr;:.......,.,.,,:::,,...............,,::.,,,,:,::,,:,:,,,:,;:
,.::,:,,,,,;;;;;;;;r;;::,..............................;;;:;::::,:::::::,:,:,,,
: ,,:,,,,,,,,,,,,,:;rrr;;:;,,,,,,,::,.,.:.,.,;s,:;;;;:;:;;;;;::::,:::,:::,:,:,:
,.,,,,,,,...,,.,,....................................:,............:,,,:,:,,,,,
Net: Detected MACID:0:c:29:4a:95:8b
Ethernet PHY: GENERIC @ 0x01
DaVinci EMAC
Hit any key to stop autoboot: 0
NAND read: device 0 offset 0x280000, size 0x440000
4456448 bytes read: OK
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-2.6.37
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2566000 Bytes = 2.4 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (root@zb205-desktop) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 Wed Feb 4 11:51:35 CST 2015
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8168evm
bootconsole [earlycon0] enabled
reserved size = 52428800 at 0x0
FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8168 2.0
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 52224
Kernel command line: console=ttyO2,115200n8 root=/dev/mtdblock3 rw rootfstype=jffs2 mem=256M earlyprintk notifyk.vpssm3_sva=0xbfd00000
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 206MB = 206MB total
Memory: 203164k/203164k available, 58980k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xd0800000 - 0xf8000000 ( 632 MB)
lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc003c000 ( 208 kB)
.text : 0xc003c000 - 0xc04da000 (4728 kB)
.data : 0xc04da000 - 0xc0522f00 ( 292 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:407
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ400
Trying to install interrupt handler for IRQ401
Trying to install interrupt handler for IRQ402
Trying to install interrupt handler for IRQ403
Trying to install interrupt handler for IRQ404
Trying to install interrupt handler for IRQ405
Trying to install interrupt handler for IRQ406
Trying to install type control for IRQ407
Trying to set irq flags for IRQ407
OMAP clockevent source: GPTIMER1 at 27000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
omap_voltage_add_dev: VDD specified does not exist!
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 0
_omap_mux_get_by_name: Could not find signal i2c2_scl.i2c2_scl
_omap_mux_get_by_name: Could not find signal i2c2_sda.i2c2_sda
NOR: Can't request GPMC CS
registered ti816x_gpio_vr device
registered ti816x_sr device
pm_dbg_init: only OMAP3 supported
registered ti81xx_vpss device
registered ti81xx_vidout device
registered ti81xx on-chip HDMI device
registered ti81xx_fb device
registered ti81xx_vin device
ti81xx_pcie: Invoking PCI BIOS...
ti81xx_pcie: Setting up Host Controller...
ti81xx_pcie: Register base mapped @0xd0820000
ti81xx_pcie: Starting PCI scan...
PCI: bus0: Fast back to back transfers enabled
bio: create slab <bio-0> at 0
regulator: VFB: 800 <--> 1025 mV at 1010 mV
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
USBSS revision 4ea20809
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
omap_i2c omap_i2c.2: bus 2 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
MUSB controller-0 revision 4ea20800
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
usb usb1: SerialNumber: musb-hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.0: USB Host mode controller at d081e000 using DMA, IRQ 18
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
MUSB controller-1 revision 4ea20800
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
usb usb2: SerialNumber: musb-hdrc.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at d0826800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
msgmni has been set to 396
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
console [ttyO2] enabled, bootconsole disabled
console [ttyO2] enabled, bootconsole disabled
brd: module loaded
loop: module loaded
ahci ahci.0: forcing PORTS_IMPL to 0x3
ahci ahci.0: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode
ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci_platform
scsi1 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16
m25p80 spi1.0: found m25p05-nonjedec, expected m25p80
m25p80 spi1.0: m25p05-nonjedec (64 Kbytes)
Creating 4 MTD partitions on "spi_flash":
0x000000000000-0x000000040000 : "U-Boot"
mtd: partition "U-Boot" extends beyond the end of device "spi_flash" -- size truncated to 0x10000
0x000000010000-0x000000012000 : "U-Boot Env"
mtd: partition "U-Boot Env" is out of reach -- disabled
0x000000000000-0x000000280000 : "Kernel"
mtd: partition "Kernel" extends beyond the end of device "spi_flash" -- size truncated to 0x10000
0x000000010000-0x000000010000 : "File System"
mtd: partition "File System" is out of reach -- disabled
omap2-nand driver initializing
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron )
Creating 5 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x00000cee0000 : "File System"
0x00000cee0000-0x000010000000 : "Reserved"
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffff9
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
davinci_mdio davinci_mdio.0: phy[2]: device 0:02, driver unknown
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver dm9601
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.0.0)
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
notify_init : notify drivercreated for remote proc id 2 at physical Address 0xbfd00000
usbcore: registered new interface driver snd-usb-audio
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
ALSA device list:
#0: TI81XX EVM
TCP cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
smartreflex smartreflex: Driver initialized
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
ata1: SATA link down (SStatus 0 SControl 300)
ata2: SATA link down (SStatus 0 SControl 300)
Division by zero in kernel.
Backtrace:
[<c004abb8>] (dump_backtrace+0x0/0x110) from [<c039d8f4>] (dump_stack+0x18/0x1c)
r7:ccabee00 r6:ccb58000 r5:00000000 r4:00000000
[<c039d8dc>] (dump_stack+0x0/0x1c) from [<c004b3ac>] (__div0+0x18/0x20)
[<c004b394>] (__div0+0x0/0x20) from [<c01b35a4>] (Ldiv0+0x8/0x10)
[<c016db08>] (jffs2_do_fill_super+0x0/0x238) from [<c016e9e8>] (jffs2_fill_super+0xbc/0xd4)
r7:00000001 r6:00000000 r5:ccabee00 r4:ccb58000
[<c016e92c>] (jffs2_fill_super+0x0/0xd4) from [<c023b5f0>] (mount_mtd_aux+0x54/0xe8)
r7:00000000 r6:00008000 r5:cca7ce00 r4:ccabee00
[<c023b59c>] (mount_mtd_aux+0x0/0xe8) from [<c023b6e0>] (mount_mtd_nr+0x5c/0x64)
r7:00008000 r6:c0501928 r5:00000000 r4:ccb52c40
[<c023b684>] (mount_mtd_nr+0x0/0x64) from [<c023b828>] (mount_mtd+0x140/0x170)
r7:c0501928 r6:00008000 r5:01f00003 r4:ccb52c40
[<c023b6e8>] (mount_mtd+0x0/0x170) from [<c016e6c0>] (jffs2_mount+0x1c/0x28)
[<c016e6a4>] (jffs2_mount+0x0/0x28) from [<c00ca658>] (vfs_kern_mount+0xac/0x1d8)
[<c00ca5ac>] (vfs_kern_mount+0x0/0x1d8) from [<c00ca7e0>] (do_kern_mount+0x3c/0xe0)
[<c00ca7a4>] (do_kern_mount+0x0/0xe0) from [<c00e0290>] (do_mount+0x68c/0x6ec)
r9:00000000 r8:ccb52c40 r7:00000020 r6:00000000 r5:00000000
r4:00008000
[<c00dfc04>] (do_mount+0x0/0x6ec) from [<c00e037c>] (sys_mount+0x8c/0xcc)
[<c00e02f0>] (sys_mount+0x0/0xcc) from [<c0008f50>] (do_mount_root+0x28/0xc0)
r7:cc814000 r6:c0072de8 r5:c002ec44 r4:cc814000
[<c0008f28>] (do_mount_root+0x0/0xc0) from [<c00091d4>] (mount_block_root+0x100/0x220)
r4:cc814000
[<c00090d4>] (mount_block_root+0x0/0x220) from [<c00093a0>] (mount_root+0xac/0xcc)
[<c00092f4>] (mount_root+0x0/0xcc) from [<c0009530>] (prepare_namespace+0x170/0x1d4)
r4:c0522f64
[<c00093c0>] (prepare_namespace+0x0/0x1d4) from [<c00087c4>] (kernel_init+0x114/0x154)
r5:c00086b0 r4:c0522f00
[<c00086b0>] (kernel_init+0x0/0x154) from [<c0072de8>] (do_exit+0x0/0x5e4)
r5:c00086b0 r4:00000000
Division by zero in kernel.
Backtrace:
[<c004abb8>] (dump_backtrace+0x0/0x110) from [<c039d8f4>] (dump_stack+0x18/0x1c)
r7:ccabee00 r6:ccb58000 r5:00000000 r4:00000000
[<c039d8dc>] (dump_stack+0x0/0x1c) from [<c004b3ac>] (__div0+0x18/0x20)
[<c004b394>] (__div0+0x0/0x20) from [<c01b35a4>] (Ldiv0+0x8/0x10)
[<c016bfcc>] (jffs2_do_mount_fs+0x0/0x648) from [<c016dc64>] (jffs2_do_fill_super+0x15c/0x238)
[<c016db08>] (jffs2_do_fill_super+0x0/0x238) from [<c016e9e8>] (jffs2_fill_super+0xbc/0xd4)
r7:00000001 r6:00000000 r5:ccabee00 r4:ccb58000
[<c016e92c>] (jffs2_fill_super+0x0/0xd4) from [<c023b5f0>] (mount_mtd_aux+0x54/0xe8)
r7:00000000 r6:00008000 r5:cca7ce00 r4:ccabee00
[<c023b59c>] (mount_mtd_aux+0x0/0xe8) from [<c023b6e0>] (mount_mtd_nr+0x5c/0x64)
r7:00008000 r6:c0501928 r5:00000000 r4:ccb52c40
[<c023b684>] (mount_mtd_nr+0x0/0x64) from [<c023b828>] (mount_mtd+0x140/0x170)
r7:c0501928 r6:00008000 r5:01f00003 r4:ccb52c40
[<c023b6e8>] (mount_mtd+0x0/0x170) from [<c016e6c0>] (jffs2_mount+0x1c/0x28)
[<c016e6a4>] (jffs2_mount+0x0/0x28) from [<c00ca658>] (vfs_kern_mount+0xac/0x1d8)
[<c00ca5ac>] (vfs_kern_mount+0x0/0x1d8) from [<c00ca7e0>] (do_kern_mount+0x3c/0xe0)
[<c00ca7a4>] (do_kern_mount+0x0/0xe0) from [<c00e0290>] (do_mount+0x68c/0x6ec)
r9:00000000 r8:ccb52c40 r7:00000020 r6:00000000 r5:00000000
r4:00008000
[<c00dfc04>] (do_mount+0x0/0x6ec) from [<c00e037c>] (sys_mount+0x8c/0xcc)
[<c00e02f0>] (sys_mount+0x0/0xcc) from [<c0008f50>] (do_mount_root+0x28/0xc0)
r7:cc814000 r6:c0072de8 r5:c002ec44 r4:cc814000
[<c0008f28>] (do_mount_root+0x0/0xc0) from [<c00091d4>] (mount_block_root+0x100/0x220)
r4:cc814000
[<c00090d4>] (mount_block_root+0x0/0x220) from [<c00093a0>] (mount_root+0xac/0xcc)
[<c00092f4>] (mount_root+0x0/0xcc) from [<c0009530>] (prepare_namespace+0x170/0x1d4)
r4:c0522f64
[<c00093c0>] (prepare_namespace+0x0/0x1d4) from [<c00087c4>] (kernel_init+0x114/0x154)
r5:c00086b0 r4:c0522f00
[<c00086b0>] (kernel_init+0x0/0x154) from [<c0072de8>] (do_exit+0x0/0x5e4)
r5:c00086b0 r4:00000000
Division by zero in kernel.
Backtrace:
[<c004abb8>] (dump_backtrace+0x0/0x110) from [<c039d8f4>] (dump_stack+0x18/0x1c)
r7:cc82a000 r6:00000080 r5:00000000 r4:00000080
[<c039d8dc>] (dump_stack+0x0/0x1c) from [<c004b3ac>] (__div0+0x18/0x20)
[<c004b394>] (__div0+0x0/0x20) from [<c01b35a4>] (Ldiv0+0x8/0x10)
[<c016bfcc>] (jffs2_do_mount_fs+0x0/0x648) from [<c016dc64>] (jffs2_do_fill_super+0x15c/0x238)
[<c016db08>] (jffs2_do_fill_super+0x0/0x238) from [<c016e9e8>] (jffs2_fill_super+0xbc/0xd4)
r7:00000001 r6:00000000 r5:ccabee00 r4:ccb58000
[<c016e92c>] (jffs2_fill_super+0x0/0xd4) from [<c023b5f0>] (mount_mtd_aux+0x54/0xe8)
r7:00000000 r6:00008000 r5:cca7ce00 r4:ccabee00
[<c023b59c>] (mount_mtd_aux+0x0/0xe8) from [<c023b6e0>] (mount_mtd_nr+0x5c/0x64)
r7:00008000 r6:c0501928 r5:00000000 r4:ccb52c40
[<c023b684>] (mount_mtd_nr+0x0/0x64) from [<c023b828>] (mount_mtd+0x140/0x170)
r7:c0501928 r6:00008000 r5:01f00003 r4:ccb52c40
[<c023b6e8>] (mount_mtd+0x0/0x170) from [<c016e6c0>] (jffs2_mount+0x1c/0x28)
[<c016e6a4>] (jffs2_mount+0x0/0x28) from [<c00ca658>] (vfs_kern_mount+0xac/0x1d8)
[<c00ca5ac>] (vfs_kern_mount+0x0/0x1d8) from [<c00ca7e0>] (do_kern_mount+0x3c/0xe0)
[<c00ca7a4>] (do_kern_mount+0x0/0xe0) from [<c00e0290>] (do_mount+0x68c/0x6ec)
r9:00000000 r8:ccb52c40 r7:00000020 r6:00000000 r5:00000000
r4:00008000
[<c00dfc04>] (do_mount+0x0/0x6ec) from [<c00e037c>] (sys_mount+0x8c/0xcc)
[<c00e02f0>] (sys_mount+0x0/0xcc) from [<c0008f50>] (do_mount_root+0x28/0xc0)
r7:cc814000 r6:c0072de8 r5:c002ec44 r4:cc814000
[<c0008f28>] (do_mount_root+0x0/0xc0) from [<c00091d4>] (mount_block_root+0x100/0x220)
r4:cc814000
[<c00090d4>] (mount_block_root+0x0/0x220) from [<c00093a0>] (mount_root+0xac/0xcc)
[<c00092f4>] (mount_root+0x0/0xcc) from [<c0009530>] (prepare_namespace+0x170/0x1d4)
r4:c0522f64
[<c00093c0>] (prepare_namespace+0x0/0x1d4) from [<c00087c4>] (kernel_init+0x114/0x154)
r5:c00086b0 r4:c0522f00
[<c00086b0>] (kernel_init+0x0/0x154) from [<c0072de8>] (do_exit+0x0/0x5e4)
r5:c00086b0 r4:00000000
VFS: Mounted root (jffs2 filesystem) on device 31:3.
devtmpfs: error mounting -2
Freeing init memory: 208K
Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
Backtrace:
[<c004abb8>] (dump_backtrace+0x0/0x110) from [<c039d8f4>] (dump_stack+0x18/0x1c)
r7:00000013 r6:c0072de8 r5:c00086b0 r4:c0523750
[<c039d8dc>] (dump_stack+0x0/0x1c) from [<c039d958>] (panic+0x60/0x17c)
[<c039d8f8>] (panic+0x0/0x17c) from [<c003c5c8>] (init_post+0xa4/0xc4)
r3:ccabab00 r2:00000000 r1:c06f2740 r0:c045bd1d
[<c003c524>] (init_post+0x0/0xc4) from [<c00087c8>] (kernel_init+0x118/0x154)
r5:c00086b0 r4:c0522f00
[<c00086b0>] (kernel_init+0x0/0x154) from [<c0072de8>] (do_exit+0x0/0x5e4)
r5:c00086b0 r4:00000000
and here are my settings:
TI8168_EVM#print
bootdelay=3
baudrate=115200
autoload=no
verify=yes
ethaddr=00:0c:29:4a:95:8b
ipaddr=192.168.1.100
nfsserver=192.168.1.108
gatewayip=192.168.1.1
netmask=255.255.255.0
hostname=zb205-desktop
addip=setenv bootargs ${bootargs} ip=${ipaddr}:${nfsserver}:${gatewayip}:${netmask}:${hostname}:eth0:off
serverip=192.168.1.108
ethact=DaVinci EMAC
bootargs=console=ttyO2,115200n8 root=/dev/mtdblock3 rw rootfstype=jffs2 mem=256M earlyprintk notifyk.vpssm3_sva=0xbfd00000
ver=U-Boot 2010.06 (Jan 30 2015 - 17:20:36)
bootcmd=nand read 0x81000000 0x00280000 0x440000; bootm;
Environment size: 561/8188 bytes
I'm really stuck here,Would you please help me?
Thanks a lot!
Bset regards!