This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ti_plugins+dm355+g711 codec

hi §
I want to encode sound coming from alsasrc(micro) with g711 codec and send it with udp+rtp over network.
I am using DM355 EVM and the last trunk from gstreamer.ti.com svn.
I tried to change the source to support speech interface, i have done some modification in this elements= "gstticodecplugin_dm355.c", "gstticodecs_dm355.c" and "gstticodecs_platform.c" but i couldn't to clone the "tiaudenc.c" to have an element which detect the speech interface.
I also found that it is easier to integrate g711 codec with ti gstreamer plugins by using diego dompe branch but i don't know which files should i change and what are the little modifications that i have to do.
I would be greatful if someone  can help me to integrate g711 codec using one of these two method.
Regards,
Seif