This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM816x GMII Not Compatible with 2.5V I/O Ethernet PHY

Hi,

As I understand, it is possible to interface Ethernet PHY whose I/O supply is 2.5V (like 88E1111) to the GMII interface of DM816x as it meets the electrical specs (Vih and Vil) of Netra at RXD side. The specs are met even if I consider the margins due to power supply noise.

Whereas in TXD side it is fine since the PHY I/Os are 3.3V tolerant.

What I don't understand is that in the DM816x Datasheet it is mentioned that "Only Ethernet PHYs with 3.3V I/Os interface should be used".

Can you please provide me the right reasoning for this?

Regards,
Shareef