This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Raw mode boot of MMC/SD of AM437x



Hi,

About Raw mode boot of MMC/SD, there is a mention in TRM of AM437x when AM437x can boot it even if I write a boot image wherever in #0, #512, #1024, #1536 of the sector of SD.
5.2.6.5.5.MMC/SD Read Sector Procedure in Raw Mode

It turns out following when I try it in EVM.
When I write in a boot image at #0, #1024 of the sector of the SD, I can boot it.
However, I cannot boot it when I write in a boot image at #512, #1536 of the sector of the SD.

It is a description error of TRM or is any setting necessary?

I assume how to use following eMMC.
#0 partition tables
#1-space
#512-boot image (EBOOT)
#1024-partition (FAT domain)

Best Regards,
shigehiro tsuda