Other Parts Discussed in Thread: OMAP3530
Hi OMAP3530 Champs,
A customer is trying to connect his GPMC to an FPGA in synchronous mode for higher throughput. He needs the GPMC_CLK signal even when not in a transaction on the GPMC bus. GPMC_CLK seems to go away when not in a transaction. Can he use SYS_CLKOUT2? It seems to be off of the CORE_DPLL but not sure if there will be a fixed constant delay.
Also is there an MTD NOR Flash driver for the OMAP3530 and does it use the FIFO/DMA? I don't see it in the Linux Kernel.
Thanks,
Jeff