Currently the HTTP server built into the TI-RTOS only supports HTTP 1.0. Are there any plans to upgrade this to 1.1?
The reason I ask is because the clients I'm using (Google chrome and Internet explorer) assume the server is 1.1 compliant, therefore it will not open a new connection each time, it will assume the connection has been left open, this causes the css file not to be successfully acquired.
If there is not currently any plans to upgrade the server, would it be possible for the server to send a transmission as soon as it is connected to a client informing it that it is HTTP 1.0?
TI-RTOS version: 2.10
NDK version: 2.24
Thanks in advance,
James