Hi,
We are running SYS/BIOS with NDK on our production board using the CPSW interface. Our current software versions:
Processor AM3352
Code Composer Version: 6.0.1.00040
Compiler TI v5.1.6
XDCTools 3.30.3.47_core
SYS/BIOS 6.40.3.39
NDK 2.24.0.11
After ~4 days of running two TCP ports to a directly connected Windows XP laptop with our software, our embedded system fails to respond to pings and our NDK stack tests fail. I will follow this post with shots of the WireShark captures and NDK internal statistics (so that the first post in this thread is not to long.)
The Laptop to Embedded system is run through a switch that mirrors the Ethernet traffic to a third laptop that captures the packets. See the following post for WireShark screen shots (I can also send the capture if you need it but it is 256Mbytes in size.)
Thanks,
John C.