This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem about dm8168 dsp alg optimize



Hi all:

I do alg optimize on dm8168 use dvrrdk4.00.

And i  want to do gauss 4x4 pyramid,

gaussDownCoef[16] = { 6, 8, 8, 6,
8, 10, 10, 8,
8, 10, 10, 8,
6, 8, 8, 6
};

and the downsample image is to do sobel, use IMG_sobel_asm in imglib from ti,

i used ping-pong buffer dma and internal mem,

and i found a strange thing is that when i split gauss  downsample and sobel in two fun and do alg optimize by each fun,

the time is less than i do in one fun, which is  IMG_sobel_asm  is done after  gauss  downsample,

i think in one fun ping-pong and dam transfer will less, so the time delay will be less,

but the i print the time delay, in one fun it cost more time,

why?

best regards

why