This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Implementation of ROI in IPNC RDK version 3.8

Hi,

I am working on ROI....Just to check how to work ROI, in your original full-feature usecase in IPNC RDK 3.8

I checked with ROI type = ROI_PRIVACY_MASK, & It works... I can see effect on streaming. (selected portion is MASKed)

But,

1. With Other Type (like - ROI_BACKGROUND_TYPE & ROI_FOREGROUND_TYPE), Not able to see effect on video or streaming. How can i do?

2. I want to also implement ROI as a CROP..... Means only selected portion is visible and other is not visible...Like reverse of ROI_FOREGROUND_TYPE.

    How can I implement ?

    Is there any patch for driver, then please provide us.

Thanks & Regards,

Sandip Gokani.