Other Parts Discussed in Thread: SYSBIOS
Hello,
We are working on dra7xx-evm(OMAP5777) board with following setup :
1. linux-3.12 kernel
2. Toolchain- gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux.
3. Filesystem- arago-glsdk-multimedia-image-dra7xx-evm.
4. glsdk_6.10.00.02
5. ipc_3_23_00_01
6. bios_6_37_03_30
7. xdctools_3_25_06_96
8. CCS5.5
We are trying to use Task_sleep(1) on DSP1 in the default project but it hangs permanently. Please find the snippet from the app.cfg file below. We are using default hal timer which is expected to produce 1ms clock-tick as default.
/*
* Create a task. The 'taskFxn' function can be found in main.c.
*/
var task0Params = new Task.Params();
var task0 = Task.create("&taskFxn", task0Params);
var Timer = xdc.useModule('ti.sysbios.
Timer.intFreq.lo = 19200000;
Clock.tickPeriod = 1000;
Clock.tickSource = Clock.TickSource_TIMER;
Clock.swiPriority = 15;
Clock.timerId = 4;
Timer.checkFrequency = true;
Please suggest to resolve the same. We don't want to configure a separate user defined timer for this purpose.
Thanks,
Naveen