Dear Engineers:
I don't know how to set/modify the uboot environment variables so that the DM3730 can boot from TFTP/NFS. The SDK is dvsdk_dm3730-evm_04_03_00_06_setuplinux. Can you help me solve the problem. Thanks!
My uboot environment variables show as follow:
bootcmd=if mmc init; then if run loadbootscript; then run bootscript; else if run loaduimage; then run mmcboot; else run nandboot; fi; fi; else run nandboot; fi
bootdelay=3
baudrate=115200
netmask=255.255.255.0
bootfile=uImage
loadaddr=0x82000000
console=ttyS0,115200n8
mpurate=1000
boardmodel=SBC37X-B2-1990-LUAC0
mmcroot=/dev/mmcblk0p2 rw
mmcrootfstype=ext3 rootwait
nandroot=ubi0:rootfs ubi.mtd=4
nandrootfstype=ubifs
nandargs=setenv bootargs console=${console} vram=${vram} omapfb.mode=dvi:${dvimode} omapfb.video_mode=dvi:${dvimode} omapdss.def_disp=${defaultdisplay} omap-dss.def_disp=${defaultdisplay} root=${nandroot} init=/init mpurate=${mpurate} boardmodel=${boardmodel} rootfstype=${nandrootfstype}
loadbootscript=fatload mmc 0 ${loadaddr} boot.scr
bootscript=echo Running bootscript from mmc ...; source ${loadaddr}
loaduimage=fatload mmc 0 ${loadaddr} uImage
mmcboot=echo Booting from mmc ...; run mmcargs; bootm ${loadaddr}
nandboot=echo Booting from nand ...; run nandargs; nand read ${loadaddr} 280000 400000; bootm ${loadaddr}
ethaddr=02:94:11:01:70:2e
dieid#=57a400029e380000016073941101702e
ethact=smc911x-0
serverip=192.168.75.194
ipaddr=192.168.75.141
gatewayip=192.168.75.11
mmcargs=setenv bootargs console=${console} vram=${vram} omapfb.vram=0:4M,1:4M omapdss.def_disp=${defaultdisplay} root=${mmcroot} init=/init mpurate=${mpurate} rootfstype=${mmcrootfstype} boardmodel=${boardmodel} mem=99M@0x80000000 mem=128M@0x88000000
displadefaultdisplay dvi
dvimode=1024x768MR-16@60
defaultdisplay=dvi
vram=12M omapfb.vram=0:12M
stdin=serial
stdout=serial
stderr=serial
Environment size: 1623/131068 bytes