Champs
My customer is trying to understand if on the X66AK2E05 device it has support for the NAND that meet the spec ONFI 3.0? On the EVM we have the 4Gb device which is compatible with the ONFI 1.0.
In the EMIF16 and the data sheet no indication as to which standard we support. The only thing that is mentioned is the ECC 1bit and 4bits only. I know other things are included in the app also but nothing about which spec we support. The only docs that have anything about ONFI stuff is the boot loader but it does not say which version we support. Also in the boot loader we mention an RBL table for compatible NAND devices but i can't find the table. If you can send out the table that would be great.
I assume we can support 8Gb device?
Thanks
regards
Mohsen