This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI CPSW 2nd ethernet port is not working

Other Parts Discussed in Thread: TPS65910Hi All , We are working on Customized Sitara board .We have successfully bring up the AM335x board with SDK 7.00.00 . We are facing some issue in TI cpsw ethernet port, one of the port is working fine and another one port is not responding. We have enabled dual EMAC support, but unable to assign interrupt in second Ethernet port. Please let me know how we can assign Interrupt to second ethernet port (i.e. eth1). Please refer the attached image of kernel messages . SDK : Version 7.00.00 Kernel : 3.12.10 Feel free for any clarifications.
  • Hi,

    There are two things to consider: The two Ethernet ports must be connected to different network segments and the second port must be brought up manually. See http://processors.wiki.ti.com/index.php/Linux_Core_CPSW_User's_Guide#Dual_Standalone_EMAC_mode for details.

  • I am attaching the kernel log .

    U-Boot SPL 2013.10 (Jan 21 2015 - 13:46:01)
    Data Out : 00000000
    Nor Pin Mux
    manufacturing ID : 93110001
    manufacturing ID_64 : 87654321

    Board is evm_sk

    SDRAM Init

    Setup Priyank
    reading args
    spl: error reading image args, err - -1
    reading u-boot.img
    reading u-boot.img


    U-Boot 2013.10 (Jan 21 2015 - 13:46:01)

    I2C: ready
    DRAM: 256 MiB
    NAND: 256 MiB
    MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
    *** Warning - bad CRC, using default environment

    Net: <ethaddr> not set. Validating first E-fuse MAC
    cpsw, usb_ether
    Hit any key to stop autoboot: 0
    U-Boot# run mmcboot
    mmc0 is current device
    SD/MMC found on device 0
    reading uEnv.txt
    ** Unable to read file uEnv.txt **
    reading zImage
    3968104 bytes read in 239 ms (15.8 MiB/s)
    reading am335x-evm.dtb
    41147 bytes read in 6 ms (6.5 MiB/s)
    Kernel image @ 0x82000000 [ 0x000000 - 0x3c8c68 ]
    ## Flattened Device Tree blob at 81000000
    Booting using the fdt blob at 0x81000000
    Loading Device Tree to 8f306000, end 8f3130ba ... OK

    Starting kernel ...

    [ 0.000000] Booting Linux on physical CPU 0x0
    [ 0.000000] Linux version 3.12.10-ti2013.12.01 (root@priyank-desktop) (gcc version 4.7.3 20135
    [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
    [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [ 0.000000] Machine: Generic AM33XX (Flattened Device Tree), model: TI AM335x EVM
    [ 0.000000] cma: CMA: reserved 24 MiB at 8d800000
    [ 0.000000] Memory policy: ECC disabled, Data cache writeback
    [ 0.000000] CPU: All CPU(s) started in SVC mode.
    [ 0.000000] AM335X ES2.1 (sgx neon )
    [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64256
    [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=extt
    [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
    [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
    [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
    [ 0.000000] Memory: 223752K/259072K available (5347K kernel code, 550K rwdata, 1784K rodata, )
    [ 0.000000] Virtual kernel memory layout:
    [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
    [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
    [ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
    [ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
    [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
    [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
    [ 0.000000] .text : 0xc0008000 - 0xc06ff04c (7133 kB)
    [ 0.000000] .init : 0xc0700000 - 0xc0755ab0 ( 343 kB)
    [ 0.000000] .data : 0xc0756000 - 0xc07df958 ( 551 kB)
    [ 0.000000] .bss : 0xc07df958 - 0xc0817ac0 ( 225 kB)
    [ 0.000000] NR_IRQS:16 nr_irqs:16 16
    [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
    [ 0.000000] Total of 128 interrupts on 1 active controller
    [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
    [ 0.000000] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms
    [ 0.000000] OMAP clocksource: timer1 at 24000000 Hz
    [ 0.000000] Console: colour dummy device 80x30
    [ 0.000294] Calibrating delay loop... 531.66 BogoMIPS (lpj=2658304)
    [ 0.049730] pid_max: default: 32768 minimum: 301
    [ 0.049826] Security Framework initialized
    [ 0.049874] Mount-cache hash table entries: 512
    [ 0.058194] CPU: Testing write buffer coherency: ok
    [ 0.058583] Setting up static identity map for 0xc053ef28 - 0xc053ef98
    [ 0.059416] devtmpfs: initialized
    [ 0.061057] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    [ 0.122074] omap_hwmod: debugss: _wait_target_disable failed
    [ 0.122757] pinctrl core: initialized pinctrl subsystem
    [ 0.123602] regulator-dummy: no parameters
    [ 0.125931] NET: Registered protocol family 16
    [ 0.127970] DMA: preallocated 256 KiB pool for atomic coherent allocations
    [ 0.130591] cpuidle: using governor ladder
    [ 0.130608] cpuidle: using governor menu
    [ 0.138503] platform mpu.1: FIXME: clock-name 'fck' DOES NOT exist in dt!
    [ 0.139512] platform 49000000.edma: FIXME: clock-name 'fck' DOES NOT exist in dt!
    [ 0.140777] OMAP GPIO hardware version 0.1
    [ 0.149679] omap-gpmc 50000000.gpmc: could not find pctldev for node /pinmux@44e10800/nandflae
    [ 0.149765] platform 50000000.gpmc: Driver omap-gpmc requests probe deferral
    [ 0.150156] platform 56000000.sgx: FIXME: clock-name 'fck' DOES NOT exist in dt!
    [ 0.154014] DSS not supported on this SoC
    [ 0.154032] No ATAGs?
    [ 0.154042] hw-breakpoint: debug architecture 0x4 unsupported.
    [ 0.174608] bio: create slab <bio-0> at 0
    [ 0.188468] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
    [ 0.189324] vbat: 5000 mV
    [ 0.189746] lis3_reg: no parameters
    [ 0.190208] wlan-en-regulator: 1800 mV
    [ 0.193327] vgaarb: loaded
    [ 0.194507] SCSI subsystem initialized
    [ 0.195806] usbcore: registered new interface driver usbfs
    [ 0.195979] usbcore: registered new interface driver hub
    [ 0.196172] usbcore: registered new device driver usb
    [ 0.197108] omap_i2c 44e0b000.i2c: could not find pctldev for node /pinmux@44e10800/pinmux_i2e
    [ 0.197137] platform 44e0b000.i2c: Driver omap_i2c requests probe deferral
    [ 0.197162] omap_i2c 4802a000.i2c: could not find pctldev for node /pinmux@44e10800/pinmux_i2e
    [ 0.197176] platform 4802a000.i2c: Driver omap_i2c requests probe deferral
    [ 0.197535] pps_core: LinuxPPS API ver. 1 registered
    [ 0.197546] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@li>
    [ 0.197675] PTP clock support registered
    [ 0.200171] Switched to clocksource timer1
    [ 0.217543] NET: Registered protocol family 2
    [ 0.218156] TCP established hash table entries: 2048 (order: 2, 16384 bytes)
    [ 0.218206] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
    [ 0.218235] TCP: Hash tables configured (established 2048 bind 2048)
    [ 0.218305] TCP: reno registered
    [ 0.218318] UDP hash table entries: 256 (order: 0, 4096 bytes)
    [ 0.218337] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    [ 0.218521] NET: Registered protocol family 1
    [ 0.218899] RPC: Registered named UNIX socket transport module.
    [ 0.218909] RPC: Registered udp transport module.
    [ 0.218916] RPC: Registered tcp transport module.
    [ 0.218923] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [ 0.219807] NetWinder Floating Point Emulator V0.97 (double precision)
    [ 0.220549] PM: Loading am335x-pm-firmware.bin
    [ 0.353605] VFS: Disk quotas dquot_6.5.2
    [ 0.353678] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    [ 0.354267] NFS: Registering the id_resolver key type
    [ 0.354356] Key type id_resolver registered
    [ 0.354364] Key type id_legacy registered
    [ 0.354404] jffs2: version 2.2. (NAND) (SUMMARY) �© 2001-2006 Red Hat, Inc.
    [ 0.354587] msgmni has been set to 485
    [ 0.356064] NET: Registered protocol family 38
    [ 0.356102] io scheduler noop registered
    [ 0.356110] io scheduler deadline registered
    [ 0.356130] io scheduler cfq registered (default)
    [ 0.358168] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
    [ 0.409753] Console: switching to colour frame buffer device 100x30
    [ 0.416516] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    [ 0.419215] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 88, base_baud = 3000000) is a OM0
    [ 1.058694] console [ttyO0] enabled
    [ 1.063248] 48022000.serial: ttyO1 at MMIO 0x48022000 (irq = 89, base_baud = 3000000) is a OM1
    [ 1.074458] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
    [ 1.090940] brd: module loaded
    [ 1.099017] loop: module loaded
    [ 1.102790] (stk) :sysfs entries created
    [ 1.106977] (stk) : debugfs entries created
    [ 1.115822] mtdoops: mtd device (mtddev=name/number) must be supplied
    [ 1.126278] Priyank: Initializing smsc911x Module
    [ 1.131390] Data Out : 00000000
    [ 1.138069] Value at address 0x894 : 00000028
    [ 1.142699] Value at address 0x878 : 0000000c
    [ 1.147315] Value of GPIO_FALLINGDETECT: 00080000
    [ 1.152303] Value of GPIO_LEVELDETECT(1): 00080000
    [ 1.157371] Value of GPIO_LEVELDETECT(1): 00080000
    [ 1.162511] Value of AM35X_GPIO_IRQSTATUS_SET(0): 00080000
    [ 1.168318] Value of AM35X_GPIO_IRQSTATUS_SET(1): 00080000
    [ 1.174153] GPIO 19 IRQ No. : 163
    [ 1.177921] Device registered 0x00000000
    [ 1.182439] smsc911x: Driver version 2008-10-21
    [ 1.187286] Priyank : Cache : 0x08000000
    [ 1.192078] manufacturing ID : 0x93110001
    [ 1.196610] Priyank : Non cache : 0xd1000000
    [ 1.201171] smsc911x smsc911x.4 (unregistered net_device): Driver Parameters:
    [ 1.208730] smsc911x smsc911x.4 (unregistered net_device): LAN base: 0xD1000000
    [ 1.216491] smsc911x smsc911x.4 (unregistered net_device): IRQ: 163
    [ 1.223137] smsc911x smsc911x.4 (unregistered net_device): PHY will be autodetected.
    [ 1.231347] Priyank : I am here
    [ 1.234770] smsc911x smsc911x.4 (unregistered net_device): BYTE_TEST: 0x87654321
    [ 1.242614] smsc911x smsc911x.4 (unregistered net_device): ID Revision: 0x93110001
    [ 1.250645] smsc911x smsc911x.4 (unregistered net_device): LAN911x identified, idrev: 0x931104
    [ 1.261505]
    [ 1.261505] IRQ _Request return value: 0
    [ 1.268083] smsc911x smsc911x.4 eth2: Network interface: "eth2"
    [ 1.274465] smsc911x smsc911x.4 eth2: External PHY is not supported, using internal PHY
    [ 1.283699] libphy: smsc911x-mdio: probed
    [ 1.287959] smsc911x smsc911x.4 eth2: PHY: addr 1, phy_id 0x00000000
    [ 1.294843] smsc911x smsc911x.4 eth2: attached PHY driver [Generic PHY] (mii_bus:phy_addr=sms)
    [ 1.305810] smsc911x smsc911x.4 eth2: Successfully verified loopback packet
    [ 1.313255] smsc911x smsc911x.4 eth2: Passed Loop Back Test
    [ 1.319156] smsc911x smsc911x.4 eth2: phy initialised successfully
    [ 1.325776] smsc911x smsc911x.4 eth2: MAC Address is set to eth_random_addr
    [ 1.333171] smsc911x smsc911x.4 eth2: MAC Address: c6:a8:cc:03:d2:fd
    [ 1.340783] usbcore: registered new interface driver asix
    [ 1.346709] usbcore: registered new interface driver ax88179_178a
    [ 1.353335] usbcore: registered new interface driver cdc_ether
    [ 1.359698] usbcore: registered new interface driver r815x
    [ 1.365678] usbcore: registered new interface driver smsc95xx
    [ 1.371939] usbcore: registered new interface driver net1080
    [ 1.378120] usbcore: registered new interface driver cdc_subset
    [ 1.384534] usbcore: registered new interface driver zaurus
    [ 1.390668] usbcore: registered new interface driver cdc_ncm
    [ 1.397170] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [ 1.404120] ehci-pci: EHCI PCI platform driver
    [ 1.409037] ehci-omap: OMAP-EHCI Host Controller driver
    [ 1.415528] usbcore: registered new interface driver cdc_wdm
    [ 1.421772] usbcore: registered new interface driver usb-storage
    [ 1.429263] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
    [ 1.436858] 44e3e000.rtc: already running
    [ 1.441881] i2c /dev entries driver
    [ 1.445744] Driver for 1-wire Dallas network protocol.
    [ 1.453497] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
    [ 1.462625] edma-dma-engine edma-dma-engine.0: allocated channel for 0:25
    [ 1.469855] edma-dma-engine edma-dma-engine.0: allocated channel for 0:24
    [ 1.477216] omap_hsmmc 48060000.mmc: unable to get vmmc regulator -517
    [ 1.484186] edma-dma-engine edma-dma-engine.0: freeing channel for 24
    [ 1.491035] edma-dma-engine edma-dma-engine.0: freeing channel for 25
    [ 1.497939] platform 48060000.mmc: Driver omap_hsmmc requests probe deferral
    [ 1.505674] edma-dma-engine edma-dma-engine.0: allocated channel for 0:13
    [ 1.512915] edma-dma-engine edma-dma-engine.0: allocated channel for 0:12
    [ 1.632141] ledtrig-cpu: registered to indicate activity on CPUs
    [ 1.640986] edma-dma-engine edma-dma-engine.0: allocated channel for 0:36
    [ 1.648277] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
    [ 1.655746] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
    [ 1.661971] edma-dma-engine edma-dma-engine.0: allocated channel for 0:5
    [ 1.669142] edma-dma-engine edma-dma-engine.0: allocated channel for 0:6
    [ 1.678809] usbcore: registered new interface driver usbhid
    [ 1.684758] usbhid: USB HID core driver
    [ 1.691100] oprofile: no performance counters
    [ 1.696097] oprofile: using timer interrupt.
    [ 1.700964] TCP: cubic registered
    [ 1.704475] Initializing XFRM netlink socket
    [ 1.709010] NET: Registered protocol family 17
    [ 1.713788] NET: Registered protocol family 15
    [ 1.718611] Key type dns_resolver registered
    [ 1.723719] cpu cpu0: cpu0 regulator not ready, retry
    [ 1.729106] platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
    [ 1.737560] ThumbEE CPU extension supported.
    [ 1.743976] omap-gpmc 50000000.gpmc: GPMC revision 6.0
    [ 1.749429] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
    [ 1.756959] ONFI param page 0 valid
    [ 1.760707] ONFI flash detected
    [ 1.764042] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron MT29F2G08ABAEAWP), 256M4
    [ 1.776135] omap2-nand: detected x8 NAND flash
    [ 1.780848] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
    [ 1.786502] omap2-nand: using custom ecc layout
    [ 1.791499] 10 ofpart partitions found on MTD device omap2-nand.0
    [ 1.797962] Creating 10 MTD partitions on "omap2-nand.0":
    [ 1.803764] 0x000000000000-0x000000020000 : "NAND.SPL"
    [ 1.810841] 0x000000020000-0x000000040000 : "NAND.SPL.backup1"
    [ 1.818359] 0x000000040000-0x000000060000 : "NAND.SPL.backup2"
    [ 1.825939] 0x000000060000-0x000000080000 : "NAND.SPL.backup3"
    [ 1.833488] 0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os"
    [ 1.841345] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot"
    [ 1.849217] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env"
    [ 1.856666] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1"
    [ 1.864831] 0x000000200000-0x000000a00000 : "NAND.kernel"
    [ 1.878389] 0x000000a00000-0x000010000000 : "NAND.file-system"
    [ 2.090895] tps65910 0-002d: No interrupt support, no core IRQ
    [ 2.099061] vrtc: 1800 mV
    [ 2.102230] vrtc: supplied by vbat
    [ 2.107075] vio: at 1500 mV
    [ 2.110216] vio: supplied by vbat
    [ 2.115058] vdd_mpu: 912 <--> 1375 mV at 1262 mV
    [ 2.120110] vdd_mpu: supplied by vbat
    [ 2.125320] vdd_core: 912 <--> 1150 mV at 1137 mV
    [ 2.130482] vdd_core: supplied by vbat
    [ 2.135468] vdd3: 5000 mV
    [ 2.139424] vdig1: at 1800 mV
    [ 2.142740] vdig1: supplied by vbat
    [ 2.147574] vdig2: at 1800 mV
    [ 2.150893] vdig2: supplied by vbat
    [ 2.155706] vpll: at 1800 mV
    [ 2.158908] vpll: supplied by vbat
    [ 2.163664] vdac: at 1800 mV
    [ 2.166870] vdac: supplied by vbat
    [ 2.171629] vaux1: at 1800 mV
    [ 2.174924] vaux1: supplied by vbat
    [ 2.179726] vaux2: at 3300 mV
    [ 2.183042] vaux2: supplied by vbat
    [ 2.187876] vaux33: at 3300 mV
    [ 2.191278] vaux33: supplied by vbat
    [ 2.196184] vmmc: 1800 <--> 3300 mV at 3300 mV
    [ 2.201126] vmmc: supplied by vbat
    [ 2.205494] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
    [ 2.214397] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 100 kHz
    [ 2.221151] edma-dma-engine edma-dma-engine.0: allocated channel for 0:25
    [ 2.228357] edma-dma-engine edma-dma-engine.0: allocated channel for 0:24
    [ 2.340195] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
    [ 2.346667] davinci_mdio 4a101000.mdio: detected phy mask fffffffc
    [ 2.354674] libphy: 4a101000.mdio: probed
    [ 2.358949] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver Atheros 8031 t
    [ 2.368746] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver Atheros 8031 t
    [ 2.379336] Detected MACID = d0:39:72:75:32:1d
    [ 2.385216] cpsw: Detected MACID = d0:39:72:75:32:1f
    [ 2.391693] omap_rtc 44e3e000.rtc: setting system clock to 2015-02-06 10:10:48 UTC (142321744)
    [ 2.404774] Waiting for root device /dev/mmcblk0p2...
    [ 2.415614] mmc1: host does not support reading read-only switch. assuming write-enable.
    [ 2.427495] mmc1: new high speed SDHC card at address aaaa
    [ 2.434085] mmcblk0: mmc1:aaaa SU04G 3.69 GiB
    [ 2.440404] mmcblk0: p1 p2 p3
    [ 2.522358] EXT4-fs (mmcblk0p2): INFO: recovery required on readonly filesystem
    [ 2.530111] EXT4-fs (mmcblk0p2): write access will be enabled during recovery
    [ 2.545915] EXT4-fs (mmcblk0p2): recovery complete
    [ 2.553242] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [ 2.561896] VFS: Mounted root (ext4 filesystem) readonly on device 179:2.
    [ 2.571614] devtmpfs: mounted
    [ 2.575314] Freeing unused kernel memory: 340K (c0700000 - c0755000)
    INIT: version 2.88 booting
    Starting udev
    [ 2.944207] udevd[849]: starting version 182
    [ 3.203045] PM: request_firmware failed
    [ 5.505016] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. .
    [ 5.752329] EXT4-fs (mmcblk0p3): warning: maximal mount count reached, running e2fsck is recod
    [ 5.921567] EXT4-fs (mmcblk0p3): recovery complete
    [ 5.926678] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)
    Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory
    bootlogd.
    [ 6.340506] EXT4-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck is recod
    [ 6.352006] EXT4-fs (mmcblk0p2): re-mounted. Opts: data=ordered
    Configuring network interfaces... [ 6.766411] net eth0: initializing cpsw version 1.12 (0)
    [ 6.775127] net eth0: phy found : id is : 0x4dd074
    [ 6.831367] net eth1: initializing cpsw version 1.12 (0)
    [ 6.840061] net eth1: phy found : id is : 0x4dd074
    done.
    Fri Feb 6 10:21:00 UTC 2015
    INIT: Entering runlevel: 5
    Starting OpenBSD Secure Shell server: sshd
    done.
    Starting syslogd/klogd: done
    Stopping Bootlog daemon: bootlogd.

    _____ _____ _ _
    | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
    | | _| .'| . | . | | __| _| . | | | -_| _| _|
    |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
    |___| |___|

    Arago Project http://arago-project.org am335x-evm ttyO0

    Arago 2013.12 am335x-evm ttyO0

    am335x-evm login: root
    root@am335x-evm:~# ifconfig
    eth0 Link encap:Ethernet HWaddr D0:39:72:75:32:1D
    inet addr:10.7.212.10 Bcast:10.7.212.255 Mask:255.255.255.0
    UP BROADCAST MULTICAST MTU:1500 Metric:1
    RX packets:0 errors:0 dropped:0 overruns:0 frame:0
    TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:1000
    RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
    Interrupt:56

    eth1 Link encap:Ethernet HWaddr D0:39:72:75:32:1F
    inet addr:10.1.101.4 Bcast:10.1.101.255 Mask:255.255.255.0
    UP BROADCAST MULTICAST MTU:1500 Metric:1
    RX packets:0 errors:0 dropped:0 overruns:0 frame:0
    TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:1000
    RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

    lo Link encap:Local Loopback
    inet addr:127.0.0.1 Mask:255.0.0.0
    UP LOOPBACK RUNNING MTU:65536 Metric:1
    RX packets:0 errors:0 dropped:0 overruns:0 frame:0
    TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:0
    RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

    root@am335x-evm:~#
    CTRL-A Z for help |115200 8N1 | NOR | Minicom 2.4 | VT102 | Offline