Other Parts Discussed in Thread: TMDSDOCKH52C1
Hi,
I'm using Code Composer 5.5.0 on TMDSDOCKH52C1. OS is Windows 8.1.
In TMDSDOCKH52C1.c it says that if you want to add a device (e.g UART), you need to use the .cfg file UI.
I have two problems:
1. I mostly can't see the .cfg file UI. All I see is the "Properties" headline with nothing else.
2. When I can see the UI, even if I add the UART device, the UART section in TMDSDOCKH52C1.c UART definition is still remarked as if the #define TI_DRIVERS_UART_INCLUDED is still 0.
Am I doing something wrong?
Regards,
Oryan