This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Am335x uart+Edma with no uart timeout interrupt

I'm working at using uart to receive data.

Code from starterware 02.00.01.01 uartecho_edma.

I enable the uart fifo with RX_DMA_THRESHOLD(1).so if there is one byte in fifo.it will be delivered by dma.i enable uart LINESTSIT and RHRIT interrupt.i enable uart dma function.i configure  edma as A synchonize and acnt(1),bcnt(65535),ccnt(1).the code goes well but with  a problem.there was no uart timeout interrupt.because  every frame  length may be variable. Timeout is very important to me.can anyone help me?