This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAD Utils error while building my application DSP C6674

Hi Sir,

While trying MAD Utils for DSP C6674, I was able to build successfully with example project given (app1 & app2). But, while I'm trying with my actual application i followed the below steps :

- Build my SYS/BIOS or RTSC Project with : dynamic & relocate option enable in compilation options

- Replaced and Renamed in default example directory as myappname.out to app_1.exe and app_2.exe

- Modified the "deployment_template_C6678.json" at "map-tool\config-files" directory as attached file.

But when the phyton mapload.py is running the below error is coming :

ERROR: xipAssignAddrToSegments() - segment: 12 in app: app1  cannot be made XIP
ERROR: assignAddrToSegments Failed in Partiton: ddr-code

 
Can some one Help.  Attached : .json file and my out file (Hope the attached files  are viewable!)

6562.files.zip
Thanks

Mani Kumar