This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using QT with DM6646 - Getting QT to use the attribute buffer

Hi,

I am working with a DM6446 EVM board. I have gotten a video feed over the composite input to show up on the screen along with QT drawing some GUI stuff. However, QT takes up the entire OSD layer and doesn't show any of the video through. I know the video is there because I've written to the attribute layer manually to clear an area and the video shows through there. Is there any way to make QT automatically update the attribute layer wherever there isn't any pixel data being written to the OSD layer? Right now, wherever I'd like it to be transparent, QT just shows a bright green.

One option I think I have is to read the buffer from the OSD layer and update the attribute layer to have a value of 0 wherever the OSD layer has a bright green... but I'd rather not have to do that manually.

Thanks,

Aditya