This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Getting issue for Scale from 2560x1920 to 1920x1080 using MpSclr

HI,

I am using IPNC-RDK 3.8.

I have try to modofy FullFeature Use-case with MPSclr to scale stream from 5MP to 2MP.

If i give 1920x1080 input  to MP_SCLR, it is working fine.

But getting error in encoder link  with input of 2560x1920.

detail log:


 [host]
********** FULL FEATURE USECASE ********

 [host] ********* Entered Tri Streaming usecase - H264 1080p @60fps + H264 D1 @30fps + MJPEG 1080p @5fps ********


 [host]  128: MCFW  : CPU Revision [ES2.1] !!!

 [host]  128: MCFW  : Detected [UNKNOWN] Board !!!

 [host]  128: MCFW  : Base Board Revision [REV A] !!!
 [m3vpss ] VPS_DCTRL_INST_0
 [m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_OUTPUT SYSTEM_DC_VENC_DVO2
 [m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_OUTPUT SYSTEM_DC_VENC_HDMI
 [m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_OUTPUT SYSTEM_DC_VENC_SD
 [m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_CLK_SRC VPS_DC_VENC_HDMI | VPS_DC_VENC_DVO2
 [m3vpss ]  4710: CAMERA: Create in progress !!!
 [m3vpss ]  Channel Num Stream 0 Ch 0 ChannelNum 0
 [m3vpss ]  Channel Num Stream 1 Ch 0 ChannelNum 1
 [m3vpss ]  4710: CAMERA: VIP0 PortA camera mode is [ 8-bit, Non-mux Embedded Sync] !!!
 [m3vpss ]  4720: CAMERA: VIP 0: VID DEC 268436736 (0x36): 0002:20202020:20202020, AUD_STATUS 538976288
 [m3vpss ] Iss_captCreate:1661
 [m3vpss ]  4724: CAMERA: Create Done !!!
 [m3vpss ]  4935: CAMERA: Detect video in progress !!!
 [m3vpss ]  4935: CAMERA: Detect video Done !!!
 [m3vpss ] DCC server task running
 [m3vpss ]  5009: MP_SCLR: Create in progress !!!
 [m3vpss ]  5011: MP_SCLR: Configured to use scalar instance 5 !!!
 [m3vpss ]  5012: MP_SCLR: Create Done !!!
 [m3vpss ]  5019: DUP   : Create Done !!!
 [m3vpss ]  DMA: ChannelID allocated:6
5025: DUP   : CrDMA: ChannelID allocated:7
eate Done !!!
 [m3vpss ]  5027: MERGE   : Create Done !!!
 [m3vpss ] {SWOSD} edma3Handle->tccVal = 36
 [m3vpss ] {SWOSD} edma3Handle->chId   = 36
 [m3vpss ] {SWOSD} edma3Handle->tccVal = 37
 [m3vpss ] {SWOSD} edma3Handle->chId   = 37
 [m3vpss ] {SWOSD} edma3Handle->tccVal = 38
 [m3vpss ] {SWOSD} edma3Handle->chId   = 38

 [host] Vsys_eventHandler:OSA_dmaOpen passed with ch id = 6

 [host] Vsys_eventHandler:OSA_dmaOpen passed with ch id = 7
 [m3vpss ]  5037: SYSTEM: Opening MsgQ [HOST_MSGQ] ...
 [m3video]  5101: IPC_IN_M3   : Create in progress !!!
 [m3vpss ]  5029: SWOSD   : Create Done !!!
 [m3video]  5101: SYSTEM: Opening ListMP [VPSS-M3_IPC_OUT_0] ...
 [m3vpss ]  5099: IPC_OUT_M3   : Create in progress !!!
 [m3video]  5102: SYSTEM: Opening ListMP [VPSS-M3_IPC_IN_0] ...
 [m3vpss ]  5101: IPC_OUT_M3   : Create Done !!!
 [m3video]  5105: IPC_IN_M3   : Create Done !!!
 [m3video]  5105: ENCODE: Create in progress ... !!!
 [m3video]  5232: ENCODE: Creating CH0 of 1920 x 1080, pitch = (3840, 32768) [PROGRESSIVE] [NON-TILED  ], bitrate = 8000 Kbps ...
 [m3video] 5314:!ERROR!:ENCLINK::links_m3video/iva_enc/encLink_h264.c:[203]::INTERNAL ERROR:-1
 [m3video] ALGCONTROL FAILED:CMD:6
 [m3video] ERROR: XDM_UNSUPPORTEDPARAM = 14,
 [m3video] ERROR: XDM_FATALERROR = 15
 [m3video] ERROR: IH264ENC_UNSUPPORTED_VIDENC2PARAMS = 20,
 [m3video] 5315:!ERROR!:ENCLINK::links_m3video/iva_enc/encLink_h264.c:[203]::INTERNAL ERROR:-1
 [m3video] ALGCONTROL FAILED:CMD:9
 [m3video] ERROR: XDM_UNSUPPORTEDPARAM = 14,
 [m3video] ERROR: XDM_FATALERROR = 15
 [m3video] ERROR: IH264ENC_UNSUPPORTED_VIDENC2PARAMS = 20,
 [m3video] 5316:!ERROR!:ENCLINK::links_m3video/iva_enc/encLink_h264.c:[203]::INTERNAL ERROR:-1
 [m3video] ALGCONTROL FAILED:CMD:3
 [m3video] ERROR: XDM_UNSUPPORTEDPARAM = 14,
 [m3video] ERROR: XDM_FATALERROR = 15
 [m3video] ERROR: IH264ENC_UNSUPPORTED_VIDENC2PARAMS = 20,
 [m3video]  
 [m3video] 5317:ERR::linkID:10000028::channelID:0::errorCode:-5::FileName:links_m3video/iva_enc/encLink_h264.c::linuNum:1235::errorCondition:(algStatus == XDM_EOK)
 [m3video]  5318: Assertion @ Line: 912 in links_m3video/iva_enc/encLink_common.c: retVal == ENC_LINK_S_SUCCESS : failed !!!
 inside autorun
 sbulla: unknown partition table
 sbulla: unknown partition table
INIT: Entering runlevel: 5
Starting telnet daemon.