Other Parts Discussed in Thread: OMAP-L137, OMAPL138
I am experimenting with some eMMC memory samples from Kingston (EMMC08G-W100-E06U).
I am running the RTFS_1_10_02_32 mmcsd example code using the Spectrum Digital OMAP-L137 EVM board. When using an SD card or micro SD card with an adapter, the example code runs perfectly.
When I substitute the eMMC chip (Kingston provided an SD card adapter board), the code doesn't work as expected. The drive seems to mount correctly and is assigned a drive letter. However, any directory or file operation return errors. Typically, the return code is 0, which seems to correspond to "no error." I'm not sure how to proceed.
I am using the CCSv4.2.4, DSP/BIOS 5.41_10_36, PSP 1_30_01.