This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[C6657EVM, BOC] BOC is available to evaluate PCIe with C6657 ?

Hi,

I would like to confirm whether BOC is available to evaluate PCIe with two C6657 EVMs.

http://processors.wiki.ti.com/index.php/CI_Dual_EVM_Break_Out_Card

In the above wiki, C6657 EVM looks unverified with BOC. Also, I found the following post and it says C6657 is not verified with BOC.

http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/368909/1297291#1297291

But on the other hand, there is a sample code of PCIe in C6657 PDK package:
<pdk_install_dir>\pdk_C6657_1_1_2_6\packages\ti\drv\pcie\example\sample

If BOC is supported for C6657 EVM, can you share the board revisions to work the PDK sample ?

Best Regards,
Kawada