Other Parts Discussed in Thread: TCI6638K2K
Hi All,
I have a query regarding Boot Parameter Table in case of booting DSP image through PCIe.
As per the Table 8-20 "PCIe Boot Parameter Table" in section "8.1.2.4.4" of TCI6638K2K datasheet(SPRS836D),there are parameters which are not Configured through Boot Pins,like Options at offset 22,SerDes cfg msw at offset 46 and SerDes cfg lsw at offset 48.So how the value of these parameters can be modified.
Is the Default Boot Parameter Table loaded by RBL sufficient to Boot application image through PCIe on TCI6638K2K?
Thanks in advance,
Chandan