This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about C6670 IPC interrupt

Guru 15520 points

Hi,

I have a questions about C6670 IPC interrupt.

I'm generating IPC interrupt by writing '1' to IPCGRx(IPC Generation Register) bit0.

The interrupt is generated from Core0 to Core1 and from Core2 to Core3.

The IPC interrupt is assigned to Interrupt Event#90.

So, when IPC was generated from Core0 and Core2 at the same time, is an exclusive access control needed?

best regards,

g.f.