Other Parts Discussed in Thread: SYSBIOS
I get the following errors when I try to build the IDK i2c_led project in the am335x_sysbios_ind_sdk_1.1.0.6. Can somebody shed some light on this. Is this a xdctools issue, sysbios or target. How do I fix this. Any help would be greatly appreciated.
Thanks.
**** Build of configuration Release for project i2c_led ****
"c:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: ../app.cfg'
'Invoking: XDCtools'
"C:/ti/xdctools_3_30_03_47_core/xs" --xdcpath="C:/ti/xdctools_3_25_06_96;c:/ti/ccsv6/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.A8Fnv -p xdc.platform.generic -r debug -c "c:/ti/ccsv6/tools/compiler/arm_5.1.6" --compileOptions "-g --optimize_with_debug" "../app.cfg"
making package.mak (because of package.bld) ...
js: "./config.bld", line 10: Error: Can't find the target named 'ti.targets.arm.elf.A8Fnv' along the path 'C:/ti/xdctools_3_25_06_96;C:/ti/ccsv6/ccs_base;C:/ti/xdctools_3_30_03_47_core/packages;..;': please check the spelling of the target's name and that it exists along this path.
xdctools_3_30_03_47_core\gmake.exe: *** No rule to make target `.configuro'. Stop.
Warning: directory "C:/ti/xdctools_3_25_06_96" on package path has a "packages" subdirectory - did you mean this instead?
js: "C:/ti/xdctools_3_30_03_47_core/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake: Target `all' not remade because of errors.
**** Build Finished ****