Other Parts Discussed in Thread: AM3356
Hi,
AM3356 -custom board .
What are the changes required for a custom board with NAND flash memory only ? I am going to modify uboot and spl shipped along with SK7.0 .
My boot configuration is
SYSBOOT[15:14] - 01b -- 24Mhz
SYSBOOT[13:12] - 00b -- reserved
SYSBOOT[11:10] - 00b -- nand boot
SYSBOOT[9] - 0b --ECC handled bu ROM
SYSBOOT[8] - dont care by rom - NC
SYSBOOT[7:6] - dont care by rom - NC
SYSBOOT[5] - 0b clock out disabled
SYSBOOT[4:0] - 10010b boot sequence NAND,NANDI2C,USB0,UART0
So ROM code will initially check for SPL [MLO binary] @0x00000000 NAND flash and execute.
I know that I have to make changes in SPL so that spl will check for uboot @0x00080000 of nand flash .
What are changes I have to do ? can anyone point out specific files in which I have to make changes ?
Thanks and regards
Gokul CG [gokul.g@kalkitech.in]