Looking through the data sheets and app notes for the C6472, I do not see any mention of whether or not there is internal termination for RGMII. Most PHYs have both input parallel and output series termination. I have seen processors to have one or the other, none, or both. What does the C6472 have?
The only info I could find was that the Hardware Design Guide requires external series resistors on the outputs. This conflicts with the EMAC Implementation Guide which shows a block diagram that does not include the series resistors. I do not see anything mentioned in the datasheet about termination for RGMII.