This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXEVM6678LE (XDS560V2) remote programming

Hi all,


I use TMDXEVM6678LE with built-in JTAG Emulator XDS560v2.  At this moment I have to change my platform configuration and need to configure remote debugging. Unfortunately my version of (built-in) XDX560v2 debugger not contains ethernet port for communication, only USB.

My question is ...is it possible to create a working configuration like this one:


HOST1 (Ubuntu PC) + TMDXEVM6678LE connected using USB

HOST2 (Ubuntu PC) + CCSv5.5 = compiling firmware + debugging target on HOST1

HOST1 and HOST2 are in the same local (Gigabit) network


Best Regards,

Damian