Other Parts Discussed in Thread: OMAP3530
hi ,
My linux kernel is 2.6.31-RC7, so which version DVSDK is matched for this kernel ?
I make the DVSDK 3.00.02.44 with 2.6.31 got so much errors.
thank you!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP3530
hi ,
My linux kernel is 2.6.31-RC7, so which version DVSDK is matched for this kernel ?
I make the DVSDK 3.00.02.44 with 2.6.31 got so much errors.
thank you!!
You must use the PSP package named
OMAP35x-PSP-SDK-setuplinux-02.01.03.11.bin
with the 3.00.02.44 DVSDK. It includes Linux kernel version: 2.6.29-rc3-omap1.
You can download these packages from here:
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/dvsdk/DVSDK_3_00/latest/index_FDS.html
This is the latest version of the DVSDK.
Regards, Clay
Thank you for your answer!
And I have other question, what is the mean of the "omap1" or "omap2" in the string of kernel version?
I konw that it refers to the "arch/arm/mach-omap1" or "arch/arm/mach-omap2",but why ?
I use the OMAP3530 , and if the OMAP3530 belongs to the "omap1" or "omap2"?
Thank you very much!!