now I met a problem:
I have a customize board based on DM6467, I want to stream video out to windows PC via usb port. so I made the following changes in the board kernel:
Kernel config for Gadget Serial Driver
[Linux Kernel Configuration] -→ [Device Drivers] -→ [USB support] -→ [USB Gadget Support]
<M> Support for USB Gadgets <M> Serial Gadget (with CDC ACM support)
then I load the gadget serial driver using command :
root@dm6467-evm:/opt/usb# insmod g_serial.ko use_acm=1
g_serial gadget: Gadget Serial v2.4
g_serial gadget: g_serial readyroot@dm6467-evm:/opt/usb# ls /dev/ttyGS0 -l
crw-rw---- 1 root dialout 250, 0 Jan 12 23:29 /dev/ttyGS0
normally,when the gadget serial driver is loaded and the USB device connected to the Windows host with a USB cable, Windows should recognize
the gadget serial device and ask for a driver. but actually,my PC had no reflection.
can anybody help me?
I already have files “gserial.inf” and “usbser.sys”.
the D- and D+ pins of USB port (B type) are connected to DN(A20) and DP(A19) pins of 6467.