This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Query regarding "Bit 9 to 11" of PCIe Boot Device Configuration Fields in TCI6638K2K datasheet(SPRS836D

Other Parts Discussed in Thread: TCI6638K2K

 The Bits 9 to 11 is shown as Reserved in the Fig 8-10 but shown as “SerDes Cfg” in Fig 8-1 of the same document datasheet TCI6638K2K?

Hi All,

In case of TCI6638K2K datasheet(SPRS836D), the bits 9 to 11 in Figure 8-10 "PCIe Boot Device Configuration Fields" has been shows as "Reserved" in case of DSP as Boot Master(Boot Master = 1),but the same Bits 9 to 11 has been shown as "SerDes Cfg"  in Fig 8.1.

Which one is correct. Please clarify.

Thanks in advance,

Regards,
Chandan