Other Parts Discussed in Thread: AM3359
Dear All
I am working with BBW running on Android JellyBean 4.1.2 (Linux kernal version 3.2) . I have one head ache with Anonymous Restart Issue .
I found that this is a known issue with Beaglebone due to some probing signals in PMIC .
Anonymous Re-start is known issue in BeagleBone running on Kernal3.2.
The root cause lies with PMIC (Power Management IC - TPS65217C) used in the system.
( PMIC is somehow confused by USB-OTG probing since it is detecting USB VBus signal and the am3359 is probing the same pin.).
Possible fixes :
- Using Angstrom 3.8 kernel
- Powering the BBB from USB
- Limiting the CPU frequency - Not efficient or convenient method .
Hardware work-around is also available as
But none of them works. Is there any possible fix or work-around possible ?