This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6713, 5-6k interface, ads1606

Other Parts Discussed in Thread: ADS1606, ADS1605

I am new to DSP programming and am trying to use the ads1606 analog converter with the C6713 through the 5-6k interface card. Through some research I came across the McBSP0 and McBSP1 but am still lost at the first step. I've tried looking at examples but they all use other ads boards or don't work for current versions of CCS (currently running v5).  Does anyone have any info about interfacing these 2 boards or can point me in the right direction to get started?

  • Hi,

    Thanks for your post.

    There is an example program which would display digitized inputs of ADS1605/1606 on the PC with DSK C6711/C6713 DSP interface, 5-6K interface card and ADS 1605/1606 EVM. Kindly refer section 4.2.1.1 for the step by step description of how to use the example program from the ADS 1605/1606 EVM user guide as below:

    http://www.ti.com/lit/ug/slau122a/slau122a.pdf

    For the TMS320C6713 DSK, Open ADS1605−C6713.pjt in the CCS v3.3  and before this, kindly make sure the jumper settings on the 5−6K interface card are set according to the Table 4−1 and Figure 4−1 mentioned in the above user guide.

    May be, you could also refer AS1606 datasheet below for interfacing ADS1606 to the C6000 devices (Refer Figure 29):

    http://www.ti.com/lit/ds/symlink/ads1606.pdf

    For more info. on sample examples on ADS1606, you can also post your queries on ADS1605/ADS1606 forum to see if there are any updated User Guides / sample software.

    Thanks & regards,

    Sivaraj K

    -------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.

    -------------------------------------------------------------------------------------------------------