Hi,
============================
BIOSUSB version : 01_10_02
test board: OMAP-L137 evm
============================
The GPIO-BANK4_5's setdata register(addr: 0x01E26068) of OMAP-L137 is always cleared by jungo_thread0,and those pins goes low. So I can't keep them high statically.
I have to use those pins to light LEDs and do other things.
I have asked this question several days ago at [http://e2e.ti.com/support/embedded/f/355/p/38669/136678.aspx#136678], and Ravi didn't resolve.
Different version, same question.
I also tested the dualrole lib, and the result is the same as host lib.
Help me,please
regards
Haoxing Li