Other Parts Discussed in Thread: SYSBIOS
I am using 6678 DSP with XDC 3.24.7.73, SYS BIOS 6.32.5.54 and Compiler c6000_7.3.4. One of the cores had an internal exception. I have hooks into the BIOS error module and XDC exception module and record the registers from the exception context.
DEFAULT 4441: <<< Core 0 detected core 7 is in abort state with code 0x0
DEFAULT 4442: <<< Core 7 Abort Msg: ti.sysbios.family.c64p.Exception: line 248: .
DEFAULT 4443: <<< Core 7 Abort ArgsInfo: ; .
DEFAULT 4444: <<< Core 7 Register log: ERF 0x2 NRP 0x0 NTSR 0x1000C IERR 0x0 A31 0x14D000 A30 0xBE4 B31 0xD4 B30 0xBD8 ITSR 0x1000C IRP 0x0 SSR 0x0 AMR 0x0 ILC 0x2 RILC 0x0.
DEFAULT 4445: <<< Core 7 Memory Exception Regs: UMC_MPFAR 0x184A280 UMC_MPFSR 0x110 PMC_MPFAR 0x0 PMC_MPFSR 0x0 DMC_MPFAR 0x184A280 DMC_MPFSR 0x120
DEFAULT 4446: <<< Core 7 Register A[0-14]: 0x0 0x0 0xABFF6914 0x0 0xABFF6910 0xFFFFFFFF 0xABFF6914 0x398 0x3F 0x2A 0x0 0xABFF5D3C 0x1 0xF9513FDF 0x88100
DEFAULT 4447: <<< Core 7 Register A[15-29]: 0x0 0x4 0xABFF656C 0xD400FD78 0x1A8 0x264011C 0x0 0xABFF5FF8 0xABFF5FE8 0xABFF5FD8 0xABFF5FE8 0xE4C 0x830E1C 0x1D 0xE4C
DEFAULT 4448: <<< Core 7 Register B[0-14]: 0x1 0x1 0x0 0x1 0xABFF6914 0xFFFFFFFF 0x0 0xFFFFFFFF 0x1 0x82DA94 0x1 0xABFF6918 0x0 0x1 0x82DF80
DEFAULT 4449: <<< Core 7 Register B[15-29]: 0x83EB68 0x264031C 0xD40001C0 0x2640310 0xFFFFFFFF 0x8622 0x0 0x8A 0x7F 0x50 0xE1 0x6B667CD2 0x0 0xBE0 0xABFF691C
An internal exception is recorded in the ERF. I see a memory protection registers caught addresses during the exception. These addresses map to internal registers of the 6678.
From the memory map:
01800000 01BFFFFF 0 01800000 0 01BFFFFF 4M C66x CorePac Registers