This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358 and NOR flash :- Booting From NOR creates LCD pin status toggle?



Question:- . While Booting from NOR flash, is there any more precaution need to be taken to interface LCD pin with AM335X 

Our customer are going to use NOR Boot and they need LCD interface.
But GPMC AD8 - AD15 and LCD DATA16 - DATA23 are using same pin so they will conflict.

Is there any solution for this?
How about changing pin mode into LCD from GPMC after NOR Boot complete?

2.
If using LCD interface, there is not enough GPMC address pin(only A0-A1) for our customer.