This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6670 Emulator minimum connections



In the documentation, there is a reference to a T! 14-pin and 20-pin header for emulator support. The 14-pin header lacks all of the advanced trace / EMU pins except for EMU0 and EMU1. The 20 pin connection adds EMU2,3 & 4. 

Question: What specific emulation or debugging features are not available when using the 14-pin or the 20-pin headers?  Also, where is additional documentation on the 14-pin header. The SPRU655i document doesn't appear to have a pin out for the 14-pin header.

Thank you.