Hi,
TI has provided the CCS interface function for us, such as connect,load,run,step,set breakpoints,clear breakpoints and so on. And we developed debugging software in the CCS based on a PCIE bus or internet, which can connect with c6678 board,can download program to the board, and debug program on the board. Now the software has been delivered to users. After they used our K1 debugging software,there are some feedback problems.
About Sysbios, because there is a conflict of our kernel and the Sysbios, so our software only realize the function of breakpoints. So could TI open source code ofSysbios and how to package the Sysbios module to us? So we can modify the sysbios modules and kernel according to the requirement of our kernel, and package into modules for users.
Thanks,
Regards