This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omapl137/da830 UART0 and UART1

Hi,

I am using omapl137/da830 , I want to use UART0 and UART1 ,but it can not work ,

smeone can tell me how to do it?

How to Setup UART0 & UART1 on OMAP-L137

thank you.

  • What software are you working ?
    Is that board was EVM or custom ?
  • Hi,

    Thanks for your post.

    It seems that the UART example is really using UART2, not UART0 and the device id in the driver properties at the tcf file really matters. So, please check the device id for the UART2 driver instance.

    May be, you could refer the bios psp uart example to setup UART instance at the below location for OMAPL137:

    C:\ti\BIOSPSP\packages\ti\pspiom\uart\build\OMAPL137\ccs3\uart.pjt

    Also, you could try to import legacy ccsv3.3 pjt to a eclipse based .ccs project too and you can build it on CCSv5.4 & run it on OMAPL137 EVM board.

    Thanks & regards,

    Sivaraj K

    -------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question

    -------------------------------------------------------------------------------------------------------

  • Thank you for your reply.

     that board is EVM.

    /*
     * TI DA8xx EVM board.
     *
     * Copyright (C) 2008-2009 MontaVista Software, Inc. <source@mvista.com>
     *
     * Derived from: arch/arm/mach-davinci/board-evm.c
     * Copyright (C) 2006 Texas Instruments.
     * Copyright (C) 2007-2008 MontaVista Software, Inc.
     *
     * This file is licensed under the terms of the GNU General Public License
     * version 2. This program is licensed "as is" without any warranty of any
     * kind, whether express or implied.
     *
     */
    #include <linux/config.h>
    #include <linux/kernel.h>
    #include <linux/serial.h>
    #include <linux/serial_8250.h>
    #include <linux/clk.h>
    #include <linux/io.h>
    #include <linux/console.h>
    #include <linux/davinci_emac.h>
    #include <linux/usb/musb.h>
    #include <linux/mtd/latch-addr-flash.h>
    #include <linux/mtd/partitions.h>
    
    #include <asm/hardware.h>
    #include <asm/mach-types.h>
    #include <asm/arch/i2c.h>
    #include <asm/mach/arch.h>
    #include <asm/arch/edma.h>
    #include <asm/arch/mux.h>
    #include <asm/arch/gpio.h>
    #include <asm/arch/clock.h>
    #include <asm/arch/nand.h>
    #include <asm/arch/common.h>
    #include <asm/arch/mmc.h>
    #include <asm/arch/usb.h>
    #include <asm/arch/da8xx_lcdc.h>
    #include <asm/arch/i2c-client.h>
    
    #include "da8xx.h"
    #include "devices.h"
    
    #define DAVINCI_DA8XX_UART_CLK		150000000
    
    #if defined(CONFIG_DA8XX_UI_NAND)
    
    static struct mtd_partition da8xx_evm_nand_partitions[] = {
    	/* bootloader (U-Boot, etc) in first sector */
    	[0] = {
    		.name		= "bootloader",
    		.offset		= 0,
    		.size		= SZ_128K,
    		.mask_flags	= MTD_WRITEABLE,	/* force read-only */
    	},
    	/* bootloader params in the next sector */
    	[1] = {
    		.name		= "params",
    		.offset		= MTDPART_OFS_APPEND,
    		.size		= SZ_128K,
    		.mask_flags	= MTD_WRITEABLE,	/* force read-only */
    	},
    	/* kernel */
    	[2] = {
    		.name		= "kernel",
    		.offset		= MTDPART_OFS_APPEND,
    		.size		= SZ_2M,
    		.mask_flags	= 0,
    	},
    	/* file system */
    	[3] = {
    		.name		= "filesystem",
    		.offset		= MTDPART_OFS_APPEND,
    		.size		= MTDPART_SIZ_FULL,
    		.mask_flags	= 0,
    	}
    };
    
    /* flash bbt decriptors */
    static uint8_t da8xx_evm_nand_bbt_pattern[] = { 'B', 'b', 't', '0' };
    static uint8_t da8xx_evm_nand_mirror_pattern[] = { '1', 't', 'b', 'B' };
    
    static struct nand_bbt_descr da8xx_evm_nand_bbt_main_descr = {
    	.options	= NAND_BBT_LASTBLOCK | NAND_BBT_CREATE |
    			  NAND_BBT_WRITE | NAND_BBT_2BIT |
    			  NAND_BBT_VERSION | NAND_BBT_PERCHIP,
    	.offs		= 2,
    	.len		= 4,
    	.veroffs	= 16,
    	.maxblocks	= 4,
    	.pattern	= da8xx_evm_nand_bbt_pattern
    };
    
    static struct nand_bbt_descr da8xx_evm_nand_bbt_mirror_descr = {
    	.options	= NAND_BBT_LASTBLOCK | NAND_BBT_CREATE |
    			  NAND_BBT_WRITE | NAND_BBT_2BIT |
    			  NAND_BBT_VERSION | NAND_BBT_PERCHIP,
    	.offs		= 2,
    	.len		= 4,
    	.veroffs	= 16,
    	.maxblocks	= 4,
    	.pattern	= da8xx_evm_nand_mirror_pattern
    };
    
    static struct nand_davinci_platform_data da8xx_evm_nand_pdata = {
    	.options	= 0,
    	.ecc_mode	= NAND_ECC_HW_SYNDROME,
    	.cle_mask	= 0x10,
    	.ale_mask	= 0x08,
    	.bbt_td		= &da8xx_evm_nand_bbt_main_descr,
    	.bbt_md		= &da8xx_evm_nand_bbt_mirror_descr,
    	.parts		= da8xx_evm_nand_partitions,
    	.nr_parts	= ARRAY_SIZE(da8xx_evm_nand_partitions),
    };
    
    #define	SZ_32K	(32 * 1024)
    
    static struct resource da8xx_evm_nand_resources[] = {
    	[0] = {		/* First memory resource is AEMIF control registers */
    		.start	= DA8XX_EMIF25_CONTROL_BASE,
    		.end	= DA8XX_EMIF25_CONTROL_BASE + SZ_32K - 1,
    		.flags	= IORESOURCE_MEM,
    	},
    	[1] = {		/* Second memory resource is NAND I/O window */
    		.start	= DA8XX_EMIF25_ASYNC_DATA_CE3_BASE,
    		.end	= DA8XX_EMIF25_ASYNC_DATA_CE3_BASE + PAGE_SIZE - 1,
    		.flags	= IORESOURCE_MEM,
    	},
    };
    
    static struct platform_device da8xx_evm_nand_device = {
    	.name		= "nand_davinci",
    	.id		= 0,
    	.dev		= {
    		.platform_data	= &da8xx_evm_nand_pdata,
    	},
    	.num_resources	= ARRAY_SIZE(da8xx_evm_nand_resources),
    	.resource	= da8xx_evm_nand_resources,
    };
    
    #elif defined(CONFIG_DA8XX_UI_NOR)
    
    #define	SZ_32K	(32 * 1024)
    
    #define NOR_WINDOW_SIZE_LOG	15
    #define NOR_WINDOW_SIZE 	(1 << NOR_WINDOW_SIZE_LOG)
    
    static struct {
    	struct clk *clk;
    	struct {
    		struct resource *res;
    		void __iomem *addr;
    	} latch, aemif;
    } da8xx_evm_nor;
    
    static void da8xx_evm_nor_set_window(unsigned long offset, void *data)
    {
    	writeb(0, da8xx_evm_nor.latch.addr +
    	       (~3UL & (offset >> (NOR_WINDOW_SIZE_LOG - 2))));
    }
    
    static void da8xx_evm_nor_done(void *data)
    {
    	if (da8xx_evm_nor.clk != NULL) {
    		clk_disable(da8xx_evm_nor.clk);
    		clk_put(da8xx_evm_nor.clk);
    		da8xx_evm_nor.clk  = NULL;
    	}
    	if (da8xx_evm_nor.latch.addr != NULL) {
    		iounmap(da8xx_evm_nor.latch.addr);
    		da8xx_evm_nor.latch.addr = NULL;
    	}
    	if (da8xx_evm_nor.latch.res != NULL) {
    		release_mem_region(DA8XX_EMIF25_ASYNC_DATA_CE3_BASE, PAGE_SIZE);
    		da8xx_evm_nor.latch.res = NULL;
    	}
    	if (da8xx_evm_nor.aemif.addr != NULL) {
    		iounmap(da8xx_evm_nor.aemif.addr);
    		da8xx_evm_nor.aemif.addr = NULL;
    	}
    	if (da8xx_evm_nor.aemif.res != NULL) {
    		release_mem_region(DA8XX_EMIF25_CONTROL_BASE, SZ_32K);
    		da8xx_evm_nor.aemif.res = NULL;
    	}
    }
    
    static int da8xx_evm_nor_init(void *data)
    {
    	/*
    	 * Turn on AEMIF clocks
    	 */
    	da8xx_evm_nor.clk = clk_get(NULL, "AEMIFCLK");
    	if (IS_ERR(da8xx_evm_nor.clk)) {
    		printk(KERN_ERR "%s: could not get AEMIF clock\n", __func__);
    		da8xx_evm_nor.clk = NULL;
    		return -ENODEV;
    	}
    	clk_enable(da8xx_evm_nor.clk);
    
    	da8xx_evm_nor.aemif.res = request_mem_region(DA8XX_EMIF25_CONTROL_BASE,
    						     SZ_32K, "AEMIF control");
    	if (da8xx_evm_nor.aemif.res == NULL) {
    		printk(KERN_ERR	"%s: could not request AEMIF control region\n",
    		       __func__);
    		da8xx_evm_nor_done(data);
    		return -EBUSY;
    	}
    
    	da8xx_evm_nor.aemif.addr = ioremap_nocache(DA8XX_EMIF25_CONTROL_BASE,
    						   SZ_32K);
    	if (da8xx_evm_nor.aemif.addr == NULL) {
    		printk(KERN_ERR	"%s: could not remap AEMIF control region\n",
    		       __func__);
    		da8xx_evm_nor_done(data);
    		return -ENOMEM;
    	}
    
    	/*
    	 * Setup AEMIF -- timings, etc.
    	 */
    
    	/* Set maximum wait cycles */
    	writel(0xff, da8xx_evm_nor.aemif.addr + ASYNC_EMIF_AWCCR);
    
    	/* Set the async memory config register for NOR flash */
    	writel(0x00300608, da8xx_evm_nor.aemif.addr + ASYNC_EMIF_A1CR);
    
    	/* Set the async memory config register for the latch */
    	writel(0x00300388, da8xx_evm_nor.aemif.addr + ASYNC_EMIF_A2CR);
    
    	/*
    	 * Setup the window to access the latch
    	 */
    	da8xx_evm_nor.latch.res =
    		request_mem_region(DA8XX_EMIF25_ASYNC_DATA_CE3_BASE, PAGE_SIZE,
    				   "DA8xx UI NOR address latch");
    	if (da8xx_evm_nor.latch.res == NULL) {
    		printk(KERN_ERR	"%s: could not request address latch region\n",
    		       __func__);
    		da8xx_evm_nor_done(data);
    		return -EBUSY;
    	}
    
    	da8xx_evm_nor.latch.addr =
    		ioremap_nocache(DA8XX_EMIF25_ASYNC_DATA_CE3_BASE, PAGE_SIZE);
    	if (da8xx_evm_nor.latch.addr == NULL) {
    		printk(KERN_ERR	"%s: could not remap address latch region\n",
    		       __func__);
    		da8xx_evm_nor_done(data);
    		return -ENOMEM;
    	}
    
    	return 0;
    }
    
    static struct mtd_partition da8xx_evm_nor_partitions[] = {
           /* bootloader (U-Boot, etc) in first 2 sectors */
           [0] = {
    	       .name           = "bootloader",
    	       .offset         = 0,
    	       .size           = SZ_128K,
    	       .mask_flags     = MTD_WRITEABLE, /* force read-only */
           },
           /* bootloader parameters in the next 1 sector */
           [1] = {
    	       .name           = "params",
    	       .offset         = MTDPART_OFS_APPEND,
    	       .size           = SZ_64K,
    	       .mask_flags     = 0,
           },
           /* kernel */
           [2] = {
    	       .name           = "kernel",
    	       .offset         = MTDPART_OFS_APPEND,
    	       .size           = SZ_2M,
    	       .mask_flags     = 0
           },
           /* file system */
           [3] = {
    	       .name           = "filesystem",
    	       .offset         = MTDPART_OFS_APPEND,
    	       .size           = MTDPART_SIZ_FULL,
    	       .mask_flags     = 0
           }
    };
    
    static struct latch_addr_flash_data da8xx_evm_nor_pdata = {
    	.width		= 1,
    	.size		= SZ_4M,
    	.init		= da8xx_evm_nor_init,
    	.done		= da8xx_evm_nor_done,
    	.set_window	= da8xx_evm_nor_set_window,
    	.nr_parts	= ARRAY_SIZE(da8xx_evm_nor_partitions),
    	.parts		= da8xx_evm_nor_partitions,
    };
    
    static struct resource da8xx_evm_nor_resource[] = {
    	[0] = {
    		.start	= DA8XX_EMIF25_ASYNC_DATA_CE2_BASE,
    		.end	= DA8XX_EMIF25_ASYNC_DATA_CE2_BASE +
    			  NOR_WINDOW_SIZE - 1,
    		.flags	= IORESOURCE_MEM,
    	},
    	[1] = {
    		.start	= DA8XX_EMIF25_ASYNC_DATA_CE3_BASE,
    		.end	= DA8XX_EMIF25_ASYNC_DATA_CE3_BASE + PAGE_SIZE - 1,
    		.flags	= IORESOURCE_MEM,
    	},
    	[2] = {
    		.start	= DA8XX_EMIF25_CONTROL_BASE,
    		.end	= DA8XX_EMIF25_CONTROL_BASE + SZ_32K - 1,
    		.flags	= IORESOURCE_MEM,
    	}
    };
    
    static struct platform_device da8xx_evm_nor_device = {
    	.name		= "latch-addr-flash",
    	.id		= 0,
    	.dev		= {
    		.platform_data	= &da8xx_evm_nor_pdata,
    	},
    	.num_resources	= ARRAY_SIZE(da8xx_evm_nor_resource),
    	.resource	= da8xx_evm_nor_resource,
    };
    
    #endif	/* CONFIG_DA8XX_UI_NOR */
    
    static struct platform_device *da8xx_evm_devices[] __initdata = {
    #if defined(CONFIG_DA8XX_UI_NAND)
    	&da8xx_evm_nand_device,
    #elif defined(CONFIG_DA8XX_UI_NOR)
    	&da8xx_evm_nor_device,
    #endif
    };
    
    static struct davinci_i2c_platform_data da8xx_evm_i2c_pdata0 = {
    	.bus_freq	= 100,
    	.bus_delay	= 0,
    };
    
    static struct musb_hdrc_platform_data da8xx_evm_usb20_pdata = {
    #if defined(CONFIG_USB_MUSB_OTG)
    	/* OTG requires a Mini-AB connector */
    	.mode		= MUSB_OTG,
    #elif defined(CONFIG_USB_MUSB_PERIPHERAL)
    	.mode		= MUSB_PERIPHERAL,
    #elif defined(CONFIG_USB_MUSB_HOST)
    	.mode		= MUSB_HOST,
    #endif
    	/* TPS2065 switch @ 5V */
    	.power		= 500 / 2,	/* actually 1 A (sustains 1.5 A) */
    	.potpgt		= (3 + 1) / 2,	/* 3 ms max */
    
    	/* REVISIT multipoint is a _chip_ capability; not board specific */
    	.multipoint	= 1,
    };
    
    #if defined(CONFIG_USB_OHCI_HCD) || defined(CONFIG_USB_OHCI_HCD_MODULE)
    
    #define ON_BD_USB_DRV	GPIO(31)	/* GPIO1[15]	*/
    #define ON_BD_USB_OVC	GPIO(36)	/* GPIO2[4]	*/
    
    static da8xx_ocic_handler_t da8xx_evm_usb_ocic_handler;
    
    static int da8xx_evm_usb_set_power(unsigned port, int on)
    {
    	gpio_set_value(ON_BD_USB_DRV, on);
    	return 0;
    }
    
    static int da8xx_evm_usb_get_power(unsigned port)
    {
    	return gpio_get_value(ON_BD_USB_DRV);
    }
    
    static int da8xx_evm_usb_get_oci(unsigned port)
    {
    	return !gpio_get_value(ON_BD_USB_OVC);
    }
    
    static irqreturn_t da8xx_evm_usb_ocic_irq(int, void *, struct pt_regs *);
    
    static int da8xx_evm_usb_ocic_notify(da8xx_ocic_handler_t handler)
    {
    	int irq 	= gpio_to_irq(ON_BD_USB_OVC);
    	int error	= 0;
    
    	if (handler != NULL) {
    		da8xx_evm_usb_ocic_handler = handler;
    
    		error = request_irq(irq, da8xx_evm_usb_ocic_irq, IRQF_DISABLED |
    				    IRQF_TRIGGER_RISING | IRQF_TRIGGER_FALLING,
    				    "OHCI over-current indicator", NULL);
    		if (error)
    			printk(KERN_ERR "%s: could not request IRQ to watch "
    			       "over-current indicator changes\n", __func__);
    	} else
    		free_irq(irq, NULL);
    
    	return error;
    }
    
    static struct da8xx_ohci_root_hub da8xx_evm_usb11_pdata = {
    	.set_power	= da8xx_evm_usb_set_power,
    	.get_power	= da8xx_evm_usb_get_power,
    	.get_oci	= da8xx_evm_usb_get_oci,
    	.ocic_notify	= da8xx_evm_usb_ocic_notify,
    
    	/* TPS2065 switch @ 5V */
    	.potpgt		= (3 + 1) / 2,	/* 3 ms max */
    };
    
    static irqreturn_t da8xx_evm_usb_ocic_irq(int irq, void *dev_id,
    					  struct pt_regs *regs)
    {
    	da8xx_evm_usb_ocic_handler(&da8xx_evm_usb11_pdata, 1);
    	return IRQ_HANDLED;
    }
    #endif /* defined(CONFIG_USB_OHCI_HCD) || defined(CONFIG_USB_OHCI_HCD_MODULE) */
    static struct emac_init_config da8xx_evm_emac_pdata = {
    	.reset_line		= 0,
    	.emac_bus_frequency	= 148500000,
    	.mdio_reset_line	= 0,
    	.mdio_bus_frequency	= 148500000,
    	.mdio_clock_frequency	= 2200000,
    	.registers_old		= 0,
    	.gigabit		= 0,
    	.phy_mode		= -1,
    };
    
    static int da8xx_evm_mmc_get_ro(int index)
    {
    	int val, status, gpio_num = 33;
    
    	status = gpio_request(gpio_num, "MMC WP\n");
    	if (status < 0) {
    		printk(KERN_WARNING "%s can not open GPIO %d\n", __func__,
    				gpio_num);
    		return 0;
    	}
    	gpio_direction_input(gpio_num);
    	val = gpio_get_value(gpio_num);
    	gpio_free(gpio_num);
    	return val;
    }
    
    static struct davinci_mmc_platform_data da8xx_evm_mmc_pdata = {
    	.mmc_clk		= "MMC_SD_CLK",
    	.rw_threshold		= 64,
    	.use_4bit_mode		= 1,
    	.use_8bit_mode		= 1,
    	.max_frq		= 50000000,
    	.pio_set_dmatrig	= 1,
    	.get_ro			= da8xx_evm_mmc_get_ro,
    };
    
    static struct da8xx_lcdc_platform_data da8xx_evm_lcdc_pdata = {
    	.lcdc_clk_name	= "LCDCTRLCLK",
    };
    
    static void *da8xx_evm_soc_pdata[DA8XX_PDEV_COUNT] __initdata = {
    	[DA8XX_PDEV_I2C_0]	= &da8xx_evm_i2c_pdata0,
    	[DA8XX_PDEV_USB_20]	= &da8xx_evm_usb20_pdata,
    	[DA8XX_PDEV_EMAC]	= &da8xx_evm_emac_pdata,
    	[DA8XX_PDEV_MMC]	= &da8xx_evm_mmc_pdata,
    	[DA8XX_PDEV_LCDC]	= &da8xx_evm_lcdc_pdata,
    };
    
    static __init void da8xx_evm_usb_init(void)
    {
    	u32 cfgchip2;
    
    	/*
    	 * Set up USB clock/mode in the CFGCHIP2 register.
    	 * FYI:  CFGCHIP2 is 0x0000ef00 initially.
    	 */
    	cfgchip2 = davinci_cfg_readl(DA8XX_CFGCHIP(2));
    
    	/* USB2.0 PHY reference clock is 24 MHz */
    	cfgchip2 &= ~CFGCHIP2_REFFREQ;
    	cfgchip2 |=  CFGCHIP2_REFFREQ_24MHZ;
    
    	/*
    	 * Select internal reference clock for USB 2.0 PHY
    	 * and use it as a clock source for USB 1.1 PHY
    	 * (this is the default setting anyway).
    	 */
    	cfgchip2 &= ~CFGCHIP2_USB1PHYCLKMUX;
    	cfgchip2 |=  CFGCHIP2_USB2PHYCLKMUX;
    
    	/*
    	 * We have to override VBUS/ID signals when MUSB is configured into the
    	 * host-only mode -- ID pin will float if no cable is connected, so the
    	 * controller won't be able to drive VBUS thinking that it's a B-device.
    	 * Otherwise, we want to use the OTG mode and enable VBUS comparators.
    	 */
    	cfgchip2 &= ~CFGCHIP2_OTGMODE;
    #ifdef	CONFIG_USB_MUSB_HOST
    	cfgchip2 |=  CFGCHIP2_FORCE_HOST;
    #else
    	cfgchip2 |=  CFGCHIP2_SESENDEN | CFGCHIP2_VBDTCTEN;
    #endif
    
    	davinci_cfg_writel(cfgchip2, DA8XX_CFGCHIP(2));
    
    #if defined(CONFIG_USB_OHCI_HCD) || defined(CONFIG_USB_OHCI_HCD_MODULE)
    
    	if (gpio_request(ON_BD_USB_DRV, "ON_BD_USB_DRV") ||
    	    gpio_request(ON_BD_USB_OVC, "ON_BD_USB_OVC")) {
    		printk(KERN_ERR "%s: could not request GPIOs for USB1 port "
    		       "power control and over-current indicator\n", __func__);
    
    		return;
    	}
    	gpio_direction_output(ON_BD_USB_DRV, 0);
    	gpio_direction_input(ON_BD_USB_OVC);
    
    	da8xx_evm_soc_pdata[DA8XX_PDEV_USB_11] = &da8xx_evm_usb11_pdata;
    
    #endif /* defined(CONFIG_USB_OHCI_HCD) || defined(CONFIG_USB_OHCI_HCD_MODULE) */
    }
    
    #ifdef	CONFIG_DA8XX_UI
    
    /*
     * Setup the MUX_MODE pin of the GPIO expander located on the UI board:
     * 0 switches AEMIF lines to LCD, 1 (default) to NAND/NOR flashes.
     */
    static __init void da8xx_evm_expander_setup(void)
    {
    #ifdef	CONFIG_DA8XX_UI_LCD
    	davinci_i2c_expander_op(MUX_MODE_DA8XX, 0);
    #endif
    }
    
    static __init int da8xx_evm_expander_validate(enum i2c_expander_pins pin)
    {
    	switch (pin) {
    	case MUX_MODE_DA8XX:
    	case SPI_MODE_DA8XX:
    		return 0;
    	default:
    		return  -EINVAL;
    	}
    }
    
    #endif	/* CONFIG_DA8XX_UI */
    
    static __init void da8xx_evm_init(void)
    {
    	int ret;
    
    	davinci_gpio_init();
    
    #ifdef	CONFIG_DA8XX_UI
    	davinci_i2c_expander.address = 0x3F;
    	davinci_i2c_expander.init_data = 0xFF;
    	davinci_i2c_expander.name = "da8xx_evm_ui_expander";
    	davinci_i2c_expander.setup = da8xx_evm_expander_setup;
    	davinci_i2c_expander.validate = da8xx_evm_expander_validate;
    #endif
    
    	da8xx_evm_usb_init();
    
    	platform_notify = davinci_serial_init;
    
    	/* Add da8xx EVM specific devices */
    	ret = platform_add_devices(da8xx_evm_devices,
    				   ARRAY_SIZE(da8xx_evm_devices));
    	if (ret)
    		printk(KERN_WARNING "DA8xx: DA8xx EVM devices not added.\n");
    
    	/* Add generic da8xx SoC devices */
    	ret = da8xx_add_devices(da8xx_evm_soc_pdata);
    	if (ret)
    		printk(KERN_WARNING "DA8xx: SoC devices not added.\n");
    }
    
    /* nFIQ are priorities 0-1, nIRQ are priorities 2-31 (with 31 being lowest) */
    static u8 da8xx_evm_default_priorities[DA8XX_N_CP_INTC_IRQ] = {
    	[IRQ_DA8XX_COMMTX]		= 7,
    	[IRQ_DA8XX_COMMRX]		= 7,
    	[IRQ_DA8XX_NINT]		= 7,
    	[IRQ_DA8XX_EVTOUT0]		= 7,
    	[IRQ_DA8XX_EVTOUT1]		= 7,
    	[IRQ_DA8XX_EVTOUT2]		= 7,
    	[IRQ_DA8XX_EVTOUT3]		= 7,
    	[IRQ_DA8XX_EVTOUT4]		= 7,
    	[IRQ_DA8XX_EVTOUT5]		= 7,
    	[IRQ_DA8XX_EVTOUT6]		= 7,
    	[IRQ_DA8XX_EVTOUT6]		= 7,
    	[IRQ_DA8XX_EVTOUT7]		= 7,
    	[IRQ_DA8XX_CCINT0]		= 7,
    	[IRQ_DA8XX_CCERRINT]		= 7,
    	[IRQ_DA8XX_TCERRINT0]		= 7,
    	[IRQ_DA8XX_AEMIFINT]		= 7,
    	[IRQ_DA8XX_I2CINT0]		= 7,
    	[IRQ_DA8XX_MMCSDINT0]		= 7,
    	[IRQ_DA8XX_MMCSDINT1]		= 7,
    	[IRQ_DA8XX_ALLINT0]		= 7,
    	[IRQ_DA8XX_RTC]			= 7,
    	[IRQ_DA8XX_SPINT0]		= 7,
    	[IRQ_DA8XX_TINT12_0]		= 7,
    	[IRQ_DA8XX_TINT34_0]		= 7,
    	[IRQ_DA8XX_TINT12_1]		= 7,
    	[IRQ_DA8XX_TINT34_1]		= 7,
    	[IRQ_DA8XX_UARTINT0]		= 7,
    	[IRQ_DA8XX_KEYMGRINT]		= 7,
    	[IRQ_DA8XX_SECINT]		= 7,
    	[IRQ_DA8XX_SECKEYERR]		= 7,
    	[IRQ_DA8XX_MPUERR]		= 7,
    	[IRQ_DA8XX_IOPUERR]		= 7,
    	[IRQ_DA8XX_BOOTCFGERR]		= 7,
    	[IRQ_DA8XX_CHIPINT0]		= 7,
    	[IRQ_DA8XX_CHIPINT1]		= 7,
    	[IRQ_DA8XX_CHIPINT2]		= 7,
    	[IRQ_DA8XX_CHIPINT3]		= 7,
    	[IRQ_DA8XX_TCERRINT1]		= 7,
    	[IRQ_DA8XX_C0_RX_THRESH_PULSE]	= 7,
    	[IRQ_DA8XX_C0_RX_PULSE]		= 7,
    	[IRQ_DA8XX_C0_TX_PULSE]		= 7,
    	[IRQ_DA8XX_C0_MISC_PULSE]	= 7,
    	[IRQ_DA8XX_C1_RX_THRESH_PULSE]	= 7,
    	[IRQ_DA8XX_C1_RX_PULSE]		= 7,
    	[IRQ_DA8XX_C1_TX_PULSE]		= 7,
    	[IRQ_DA8XX_C1_MISC_PULSE]	= 7,
    	[IRQ_DA8XX_MEMERR]		= 7,
    	[IRQ_DA8XX_GPIO0]		= 7,
    	[IRQ_DA8XX_GPIO1]		= 7,
    	[IRQ_DA8XX_GPIO2]		= 7,
    	[IRQ_DA8XX_GPIO3]		= 7,
    	[IRQ_DA8XX_GPIO4]		= 7,
    	[IRQ_DA8XX_GPIO5]		= 7,
    	[IRQ_DA8XX_GPIO6]		= 7,
    	[IRQ_DA8XX_GPIO7]		= 7,
    	[IRQ_DA8XX_GPIO8]		= 7,
    	[IRQ_DA8XX_I2CINT1]		= 7,
    	[IRQ_DA8XX_LCDINT]		= 7,
    	[IRQ_DA8XX_UARTINT1]		= 7,
    	[IRQ_DA8XX_MCASPINT]		= 7,
    	[IRQ_DA8XX_ALLINT1]		= 7,
    	[IRQ_DA8XX_SPINT1]		= 7,
    	[IRQ_DA8XX_UHPI_INT1]		= 7,
    	[IRQ_DA8XX_USB_INT]		= 7,
    	[IRQ_DA8XX_IRQN]		= 7,
    	[IRQ_DA8XX_RWAKEUP]		= 7,
    	[IRQ_DA8XX_UARTINT2]		= 7,
    	[IRQ_DA8XX_DFTSSINT]		= 7,
    	[IRQ_DA8XX_EHRPWM0]		= 7,
    	[IRQ_DA8XX_EHRPWM0TZ]		= 7,
    	[IRQ_DA8XX_EHRPWM1]		= 7,
    	[IRQ_DA8XX_EHRPWM1TZ]		= 7,
    	[IRQ_DA8XX_EHRPWM2]		= 7,
    	[IRQ_DA8XX_EHRPWM2TZ]		= 7,
    	[IRQ_DA8XX_ECAP0]		= 7,
    	[IRQ_DA8XX_ECAP1]		= 7,
    	[IRQ_DA8XX_ECAP2]		= 7,
    	[IRQ_DA8XX_EQEP0]		= 7,
    	[IRQ_DA8XX_EQEP1]		= 7,
    	[IRQ_DA8XX_T12CMPINT0_0]	= 7,
    	[IRQ_DA8XX_T12CMPINT1_0]	= 7,
    	[IRQ_DA8XX_T12CMPINT2_0]	= 7,
    	[IRQ_DA8XX_T12CMPINT3_0]	= 7,
    	[IRQ_DA8XX_T12CMPINT4_0]	= 7,
    	[IRQ_DA8XX_T12CMPINT5_0]	= 7,
    	[IRQ_DA8XX_T12CMPINT6_0]	= 7,
    	[IRQ_DA8XX_T12CMPINT7_0]	= 7,
    	[IRQ_DA8XX_T12CMPINT0_1]	= 7,
    	[IRQ_DA8XX_T12CMPINT1_1]	= 7,
    	[IRQ_DA8XX_T12CMPINT2_1]	= 7,
    	[IRQ_DA8XX_T12CMPINT3_1]	= 7,
    	[IRQ_DA8XX_T12CMPINT4_1]	= 7,
    	[IRQ_DA8XX_T12CMPINT5_1]	= 7,
    	[IRQ_DA8XX_T12CMPINT6_1]	= 7,
    	[IRQ_DA8XX_T12CMPINT7_1]	= 7,
    	[IRQ_DA8XX_ARMCLKSTOPREQ]	= 7,
    };
    
    static __init void da8xx_evm_irq_init(void)
    {
    	da8xx_irq_init(da8xx_evm_default_priorities);
    }
    
    #ifdef CONFIG_DAVINCI_MUX
    
    /*
     * UI board NAND/NOR flashes only use 8-bit data bus.
     */
    static const short evm_emif25_pins[] = {
    	DA8XX_EMA_D_0, DA8XX_EMA_D_1, DA8XX_EMA_D_2, DA8XX_EMA_D_3,
    	DA8XX_EMA_D_4, DA8XX_EMA_D_5, DA8XX_EMA_D_6, DA8XX_EMA_D_7,
    	DA8XX_EMA_A_0, DA8XX_EMA_A_1, DA8XX_EMA_A_2, DA8XX_EMA_A_3,
    	DA8XX_EMA_A_4, DA8XX_EMA_A_5, DA8XX_EMA_A_6, DA8XX_EMA_A_7,
    	DA8XX_EMA_A_8, DA8XX_EMA_A_9, DA8XX_EMA_A_10, DA8XX_EMA_A_11,
    	DA8XX_EMA_A_12, DA8XX_EMA_BA_0, DA8XX_EMA_BA_1, DA8XX_NEMA_WE,
    	DA8XX_NEMA_CS_2, DA8XX_NEMA_CS_3, DA8XX_NEMA_OE, DA8XX_EMA_WAIT_0,
    	-1
    };
    
    /*
     * GPIO2[1] is used as MMC_SD_WP and GPIO2[2] as MMC_SD_INS.
     */
    static const short evm_mmc_sd_pins[] = {
    	DA8XX_MMCSD_DAT_0, DA8XX_MMCSD_DAT_1, DA8XX_MMCSD_DAT_2,
    	DA8XX_MMCSD_DAT_3, DA8XX_MMCSD_DAT_4, DA8XX_MMCSD_DAT_5,
    	DA8XX_MMCSD_DAT_6, DA8XX_MMCSD_DAT_7, DA8XX_MMCSD_CLK,
    	DA8XX_MMCSD_CMD,   DA8XX_GPIO2_1,     DA8XX_GPIO2_2,
    	-1
    };
    
    /*
     * UART0 is not used on the EVM board.
     * Due to the pin conflicts, evm_uart0_pins[] is empty.
     */
    static const short evm_uart0_pins[] = {
    	-1
    };
    
    /*
     * USB_REFCLKIN is not used on the EVM board.
     */
    static const short evm_usb20_pins[] = {
    	DA8XX_USB0_DRVVBUS,
    	-1
    };
    
    /*
     * USB1 VBUS is controlled by GPIO1[15], over-current is reported on GPIO2[4].
     */
    static const short evm_usb11_pins[] = {
    	DA8XX_GPIO1_15, DA8XX_GPIO2_4,
    	-1
    };
    
    static const short evm_mcasp0_pins[] = {
    	DA8XX_AXR0_9, DA8XX_AFSR0, DA8XX_ACLKR0,
    	-1
    };
    
    static const short evm_mcasp1_pins[] = {
    	DA8XX_AHCLKX1, DA8XX_ACLKX1, DA8XX_AFSX1, DA8XX_AHCLKR1, DA8XX_AFSR1,
    	DA8XX_AMUTE1, DA8XX_AXR1_0, DA8XX_AXR1_1, DA8XX_AXR1_2, DA8XX_AXR1_5,
    	DA8XX_ACLKR1, DA8XX_AXR1_6, DA8XX_AXR1_7, DA8XX_AXR1_8, DA8XX_AXR1_10,
    	DA8XX_AXR1_11,
    	-1
    };
    
    static const short evm_mcasp2_pins[] = {
    	DA8XX_AXR2_0,
    	-1
    };
    
    /*
     * GPIO3[10] is used for SPI1 chip select instead of NSPI1_ENA due to the pin
     * conflicts with UART2.
     */
    static const short evm_spi1_pins[] = {
    	DA8XX_SPI1_SOMI_0, DA8XX_SPI1_SIMO_0, DA8XX_SPI1_CLK, DA8XX_GPIO3_10,
    	-1
    };
    
    /*
     * I2C1_SCL and I2C1_SDA are not used on the EVM board.  Both are removed due
     * to SPI1_SOMI_0 vs I2C1_SCL pin conflict.
     */
    static const short evm_i2c_pins[] = {
    	DA8XX_I2C0_SDA, DA8XX_I2C0_SCL,
    	-1
    };
    
    /*
     * UART1 is not used on the EVM board.
     * Due to the pin conflicts, evm_uart1_pins[] is empty.
     */
    static const short evm_uart1_pins[] = {
    	-1
    };
    
    static void da8xx_evm_pinmux_override(void)
    {
    	da8xx_psc0_pins[DA8XX_LPSC0_EMIF25] = evm_emif25_pins;
    	da8xx_psc0_pins[DA8XX_LPSC0_MMC_SD] = evm_mmc_sd_pins;
    
    	da8xx_psc0_pins[DA8XX_LPSC0_UART0] = evm_uart0_pins;
    	da8xx_psc1_pins[DA8XX_LPSC1_UART1] = evm_uart1_pins;
    
    	da8xx_psc1_pins[DA8XX_LPSC1_USB20] = evm_usb20_pins;
    	da8xx_psc1_pins[DA8XX_LPSC1_USB11] = evm_usb11_pins;
    
    	da8xx_psc1_pins[DA8XX_LPSC1_McASP0] = evm_mcasp0_pins;
    	da8xx_psc1_pins[DA8XX_LPSC1_McASP1] = evm_mcasp1_pins;
    	da8xx_psc1_pins[DA8XX_LPSC1_McASP2] = evm_mcasp2_pins;
    
    	da8xx_psc1_pins[DA8XX_LPSC1_SPI1] = evm_spi1_pins;
    
    	da8xx_psc1_pins[DA8XX_LPSC1_I2C] = evm_i2c_pins;
    }
    #else
    static inline void da8xx_evm_pinmux_override(void) {}
    #endif /* CONFIG_DAVINCI_MUX */
    
    static __init void da8xx_evm_psc_init(void)
    {
    	davinci_psc_config(DAVINCI_GPSC_ARMDOMAIN, 0, DA8XX_LPSC0_TPCC, 1);
    	davinci_psc_config(DAVINCI_GPSC_ARMDOMAIN, 0, DA8XX_LPSC0_TPTC0, 1);
    	davinci_psc_config(DAVINCI_GPSC_ARMDOMAIN, 0, DA8XX_LPSC0_TPTC1, 1);
    	davinci_psc_config(DAVINCI_GPSC_ARMDOMAIN, 0, DA8XX_LPSC0_AINTC, 1);
    	davinci_psc_config(DAVINCI_GPSC_ARMDOMAIN, 0, DA8XX_LPSC0_ARM_RAM_ROM,
    			   1);
    	davinci_psc_config(DAVINCI_GPSC_ARMDOMAIN, 0, DA8XX_LPSC0_SECU_MGR, 1);
    	davinci_psc_config(DAVINCI_GPSC_ARMDOMAIN, 0, DA8XX_LPSC0_SCR0_SS, 1);
    	davinci_psc_config(DAVINCI_GPSC_ARMDOMAIN, 0, DA8XX_LPSC0_SCR1_SS, 1);
    	davinci_psc_config(DAVINCI_GPSC_ARMDOMAIN, 0, DA8XX_LPSC0_SCR2_SS, 1);
    	davinci_psc_config(DAVINCI_GPSC_ARMDOMAIN, 0, DA8XX_LPSC0_DMAX, 1);
    #if defined(CONFIG_TI_CPPI41) || defined(CONFIG_TI_CPPI41_MODULE)
    	davinci_psc_config(DAVINCI_GPSC_ARMDOMAIN, 1, DA8XX_LPSC1_USB20, 1);
    #endif
    #ifdef	CONFIG_INPUT_EQEP
    	davinci_psc_config(DAVINCI_GPSC_ARMDOMAIN, 1, DA8XX_LPSC1_EQEP, 1);
    #endif
    }
    
    static void __init da8xx_evm_map_io(void)
    {
    	da8xx_evm_pinmux_override();
    	da8xx_map_common_io();
    
    	/* UART clock needs to be ready otherwise kgdbwait won't work */
    	da8xx_uart_clk_init(DAVINCI_DA8XX_UART_CLK);
    	da8xx_kgdb_init();
    
    	/* Initialize the DA8XX EVM board settigs */
    	da8xx_init_common_hw();
    	da8xx_evm_psc_init();
    }
    
    #ifdef CONFIG_SERIAL_8250_CONSOLE
    static int __init da8xx_evm_console_init(void)
    {
    	return add_preferred_console("ttyS", 2, "115200");
    }
    console_initcall(da8xx_evm_console_init);
    #endif
    
    MACHINE_START(DA8XX_EVM, "DaVinci DA8XX EVM")
    	.phys_io	=  IO_PHYS,
    	.io_pg_offst	= (IO_VIRT >> 18) & 0xfffc,
    	.boot_params	= DA8XX_DDR_BASE + 0x100,
    	.map_io		= da8xx_evm_map_io,
    	.init_irq	= da8xx_evm_irq_init,
    	.timer		= &davinci_timer,
    	.init_machine	= da8xx_evm_init,
    MACHINE_END
    

  • Thank you for your answer,but can you make it clear,I can not understand it clearly. Thank you very much!!
  • Hi,

    What is your kernel version and what is the TI SDK version ?

    You have to pinmux the UART0 and UART1 and then do a platform register for that UART0 and UART1.
    Please modify the "da830.c", "serial.c" and "devices-da8xx.c" in the following location.

    arch/arm/mach-davinci

    Please note that UART0 is muxed with I2C0 and UARt1 is muxed with McASP pins so you have to disable the I2C0 peripheral and McASP in case if you want to enable both UART0 and UART1.