This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x SYSBOOT pins are LCDDATA[15:0] pins how to configure it for Boot selection



We are refering Beagle Bone Schematic where SYSBOOT pins are connected with the LCD DATA pins,

we dont want to add Two DIP switches, because in our design we have SPI  NOR Flash used for Bootloader, and NAND flash for the Kernel and RFS file.

ROM code will read Bootloader then jumped to NAND flash and copying files from NAND to DDR RAM

pls suggest two DIP switches required or not?

How to set Boot sequence for SPI NOR then NAND flash and then Micro SD / MMC card.