This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

reboot command fails with cpufreq

Guru 20755 points

Other Parts Discussed in Thread: OMAP3530

Hello,

We are using OMAP3530 , with cpufreq with perfomance governer - it all function OK.

We wanted to move to demand (or conservative) governer, but on moving to these governer,  it seems to work just fine, but we then see that the "reboot" command does not reboot the system any more.

Has anyone tried to use these governers ?

We also noticed that only in the highest frequenct 600000 (this is the frequency we always used in the past) 0 the reboot command works.

It seems that when the frequency is changed to lower value - reboot command fails to function any more !

Regards,

Ran