Other Parts Discussed in Thread: OMAP3530
Dear All, I have this question about the OMAP 423 BGA CUS package. According to the OMAP datasheet for the OMAP35x devices, the CUS package has the BGA pins on the bottom side. I want to ask, then how is the special POP memory which is used in the OMAP devices interfaced, when all the pins are at the bottom of the CUS package? or am I mistaken and it is not so, and thus it has memory interface pins for the POP packages on the top like the the other package configurations. Thank you.