Other Parts Discussed in Thread: AM1806, OMAPL138
Hi, everyone,
I have a problem of the initialization of DDR memory in the following environment.
Processor : OMAP L-138 and AM1806
Memory : DDR2
Boot mode : SPI0
PLL0 Settings : CPU(372 MHz) Pre-Divisor=2, Multiplier=31, Post-Divisor=1, DIV1=1, DIV3=16, DIV7=8
PLL1 Settings : DDR(312MHz) Multiplier=13, Post-Divisor=1, DIV1=1, DIV2=2, DIV3=3
DDR memory is driven with 156MHz.
There is a check-box "Use direct clock from PLL1" in the DDR setting tab.
If I check it , our board failed to boot once time in 300 times.
If I don't check it, our board never fail.
But the 2X_CLK should be same to DDR memory because PLL1 Post-Divisor is 1.
(1)What register is changed by "Use direct clock from PLL1" check box.
(2)This option can be used ?
Thank you for your help!!!