I have been toying with the TCP Echo example using TI-RTOS to continuously send packets of 1024 bytes (would like to increase to 1460 when working). What is happening though is I'm getting 2 smaller packets sent instead of just the one 1024 byte packet.
Setting a breakpoint on the send function and looping a send at a time seems to work most of the time however.
From Wireshark:
72428 22.591278000 192.168.0.2 192.168.0.1 TCP 490 1234→50914 [PSH, ACK] Seq=24717901 Ack=1 Win=1024 Len=436
72429 22.592141000 192.168.0.2 192.168.0.1 TCP 642 1234→50914 [PSH, ACK] Seq=24718337 Ack=1 Win=1024 Len=588
72430 22.592196000 192.168.0.1 192.168.0.2 TCP 54 50914→1234 [ACK] Seq=1 Ack=24718925 Win=63216 Len=0
My code is as follows:
I have tried to add TCP_NODELAY by adding the following:
setsockopt(server, IPPROTO_TCP, TCP_NODELAY, (void *)&i, sizeof(i));
Anyone have any ideas why the 1024 Byte packets is being split?
Regards,
Lee.
/*
* ======== tcpEcho.c ========
* Contains BSD sockets code.
*/
#include <string.h>
#include <xdc/std.h>
#include <xdc/cfg/global.h>
#include <xdc/runtime/Error.h>
#include <xdc/runtime/System.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/drivers/GPIO.h>
/* NDK BSD support */
#include <sys/socket.h>
/* Example/Board Header file */
#include "Board.h"
#define TCPPACKETSIZE 1024
#define NUMTCPWORKERS 1
const static char buffer[1024] = {
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9',
'0','1','2','3','4','5','6','7','8','9','0','1','2','3','4','5','6','7','8','9'
};
/*
* ======== tcpWorker ========
* Task to handle TCP connection. Can be multiple Tasks running
* this function.
*/
Void tcpWorker(UArg arg0, UArg arg1)
{
int clientfd = (int)arg0;
//int bytesRcvd;
int bytesSent;
// char buffer[TCPPACKETSIZE];
System_printf("tcpWorker: start clientfd = 0x%x\n", clientfd);
System_flush();
// while ((bytesRcvd = recv(clientfd, buffer, TCPPACKETSIZE, 0)) > 0) {
while(1){
bytesSent = send(clientfd, buffer,TCPPACKETSIZE, 0);
if (bytesSent < 0 ) {
System_printf("Error: send failed.\n");
System_flush();
break;
}
}
System_printf("tcpWorker stop clientfd = 0x%x\n", clientfd);
System_flush();
close(clientfd);
}
/*
Void tcpWorker(UArg arg0, UArg arg1)
{
int clientfd = (int)arg0;
int bytesRcvd;
int bytesSent;
char buffer[TCPPACKETSIZE];
System_printf("tcpWorker: start clientfd = 0x%x\n", clientfd);
while ((bytesRcvd = recv(clientfd, buffer, TCPPACKETSIZE, 0)) > 0) {
bytesSent = send(clientfd, buffer, bytesRcvd, 0);
if (bytesSent < 0 || bytesSent != bytesRcvd) {
System_printf("Error: send failed.\n");
break;
}
}
System_printf("tcpWorker stop clientfd = 0x%x\n", clientfd);
close(clientfd);
}
*/
/*
* ======== tcpHandler ========
* Creates new Task to handle new TCP connections.
*/
Void tcpHandler(UArg arg0, UArg arg1)
{
int status;
int clientfd;
int server;
struct sockaddr_in localAddr;
struct sockaddr_in clientAddr;
int optval;
int optlen = sizeof(optval);
socklen_t addrlen = sizeof(clientAddr);
Task_Handle taskHandle;
Task_Params taskParams;
Error_Block eb;
int i = 1;
server = socket(AF_INET, SOCK_STREAM, IPPROTO_TCP);
if (server == -1) {
System_printf("Error: socket not created.\n");
goto shutdown;
}
memset(&localAddr, 0, sizeof(localAddr));
localAddr.sin_family = AF_INET;
localAddr.sin_addr.s_addr = htonl(INADDR_ANY);
localAddr.sin_port = htons(arg0);
status = bind(server, (struct sockaddr *)&localAddr, sizeof(localAddr));
if (status == -1) {
System_printf("Error: bind failed.\n");
goto shutdown;
}
status = listen(server, NUMTCPWORKERS);
if (status == -1) {
System_printf("Error: listen failed.\n");
goto shutdown;
}
if (setsockopt(server, SOL_SOCKET, SO_KEEPALIVE, &optval, optlen) < 0) {
System_printf("Error: setsockopt failed\n");
goto shutdown;
}
setsockopt(server, IPPROTO_TCP, TCP_NODELAY, (void *)&i, sizeof(i));
while ((clientfd =
accept(server, (struct sockaddr *)&clientAddr, &addrlen)) != -1) {
System_printf("tcpHandler: Creating thread clientfd = %d\n", clientfd);
/* Init the Error_Block */
Error_init(&eb);
/* Initialize the defaults and set the parameters. */
Task_Params_init(&taskParams);
taskParams.arg0 = (UArg)clientfd;
taskParams.stackSize = 2560;
taskHandle = Task_create((Task_FuncPtr)tcpWorker, &taskParams, &eb);
if (taskHandle == NULL) {
System_printf("Error: Failed to create new Task\n");
close(clientfd);
}
/* addrlen is a value-result param, must reset for next accept call */
addrlen = sizeof(clientAddr);
}
System_printf("Error: accept failed.\n");
shutdown:
if (server > 0) {
close(server);
}
}
/*
* ======== main ========
*/
int main(void)
{
/* Call board init functions */
Board_initGeneral();
Board_initGPIO();
Board_initEMAC();
System_printf("Starting the TCP Echo example\nSystem provider is set to "
"SysMin. Halt the target to view any SysMin contents in"
" ROV.\n");
/* SysMin will only print to the console when you call flush or exit */
System_flush();
/* Start BIOS */
BIOS_start();
return (0);
}
/*
* ======== tcpEcho.cfg ========
*/
/* ================ General configuration ================ */
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var Diags = xdc.useModule('xdc.runtime.Diags');
var Error = xdc.useModule('xdc.runtime.Error');
var Log = xdc.useModule('xdc.runtime.Log');
var Main = xdc.useModule('xdc.runtime.Main');
var Memory = xdc.useModule('xdc.runtime.Memory');
var System = xdc.useModule('xdc.runtime.System');
var Text = xdc.useModule('xdc.runtime.Text');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
var Task = xdc.useModule('ti.sysbios.knl.Task');
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
var Hwi = xdc.useModule('ti.sysbios.hal.Hwi');
var HeapMem = xdc.useModule('ti.sysbios.heaps.HeapMem');
var LoggingSetup = xdc.useModule('ti.uia.sysbios.LoggingSetup');
BIOS.heapSize = 20480;
Task.idleTaskStackSize = 768;
/*
* Program.stack is ignored with IAR. Use the project options in
* IAR Embedded Workbench to alter the system stack size.
*/
if (!Program.build.target.$name.match(/iar/)) {
/*
* Reducing the system stack size (used by ISRs and Swis) to reduce
* RAM usage.
*/
Program.stack = 2048;
}
/* ================ System configuration ================ */
var SysMin = xdc.useModule('xdc.runtime.SysMin');
SysMin.bufSize = 128;
System.SupportProxy = SysMin;
/* Enable Semihosting for GNU targets to print to CCS console */
if (Program.build.target.$name.match(/gnu/)) {
var SemiHost = xdc.useModule('ti.sysbios.rts.gnu.SemiHostSupport');
}
/* ================ NDK configuration ================ */
var Ndk = xdc.loadPackage('ti.ndk.config');
var Global = xdc.useModule('ti.ndk.config.Global');
var Ip = xdc.useModule('ti.ndk.config.Ip');
var Udp = xdc.useModule('ti.ndk.config.Udp');
var Tcp = xdc.useModule('ti.ndk.config.Tcp');
Global.IPv6 = false;
Global.stackLibType = Global.MIN;
Global.networkOpenHook = "&netOpenHook";
/* automatically call fdOpen/CloseSession for our sockets Task */
Global.autoOpenCloseFD = true;
Global.pktNumFrameBufs = 10;
Global.memRawPageCount = 6;
Global.ndkThreadStackSize = 1536;
Global.lowTaskStackSize = 2048;
Global.normTaskStackSize = 2048;
Global.highTaskStackSize = 2048;
Tcp.transmitBufSize = 1460;
Tcp.receiveBufSize = 1024;
/* ================ Driver configuration ================ */
var TIRTOS = xdc.useModule('ti.tirtos.TIRTOS');
TIRTOS.useEMAC = true;
TIRTOS.useGPIO = true;
Ip.autoIp = false;
Ip.address = "192.168.0.2";
Tcp.maxNumReasmPkts = 1;
LoggingSetup.loadTaskLogging = true;
LoggingSetup.enableTaskProfiler = true;
Ip.socketBufMinRxSize = 100;