Other Parts Discussed in Thread: OMAPL138
Hi everyone,
We use the OMAPL138,the Boot Mode is Nand Boot Modes. The Bootloader curing in ROM guide our u - Boot (user Boot) to run. After u - the Boot running,transfer to our application. Generation and burning block numbers of u - Boot See note.
After our application run normally period of time, OMAPL138 Bootloader is unable to guide our u-Boot, cause the system can not run normally. To further investigate the problem, we want to get the reason of Bootloader curing in ROM Can't guide u – Boot and the error code of Bootloader guides unSuccessfully , please inform.
Note:
1、u - Boot generated by AISgen;
2、The same u – Boot burn on the first five Block(1, 2, 3, 4, 5) of Nandflash.