This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAD UTILITIES

Hi,

I am working on mad utilities. I was able to use image processing demo and regenerate .bin file using bypass prelink json file and was able to see the results (ip address) on UART terminal. I followed this link http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/218188/769809#769809 and was able to generate .bin file for helloworld  using bypass prelink json file . This bin also displayed helloworld in uart terminal. But I have used application in only one core. Now when I loaded application in multiple cores, the bin file was generated but it could not display any results in UART terminal. How to display helloworld from different cores.

Thanks and Regards, Nithin B