This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIF2 Rx Flow Mapping with RRH

Hi,

I have an issue with AIF2 Rx Flow Number and Radio Remote Head antenna no. Here is my setup and problem:

AIF2: One Link 20 MHz BW and 4x link rate so it has 2 AxC and RRH specs are 20 MHz and 4x Link rate. RRH has 2 antenna ports and 1 SFP port. Signal generator is connected to the first antenna of the RRH to supply data to DSP. When I run the system sometimes the signal comes from the  second AxC. AIF2 should do 1:1 mapping with AxC number with RRH antenna port, But for my case sometimes RRH Antenna port 0 sends the data into AIF2 AxC1. This issue only happens when the system start, and it is random. When I look at the descriptor PS word I can see the AxC1 but the data should not come into AxC1 because signal is coming from RRH antenna port 0. it should go to AIF2 AxC0.

I check the Rx flow settings and link configuration and I have also compared that with LTE example project, however I could not get the problem.

Please let me know If you guys have any idea about this issue.

Thanks,

Mustafa