This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

compile error while linking VLIB

Other Parts Discussed in Thread: DM3730

HI,

I have migrated my project from omap3730 to 8148.

when i compile servers in the path "/opt/ezsdk/component-sources/codec_engine_3_22_01_06/examples/ti/sdo/ce/examples/servers/face_detection", I getsome errors

 undefined                                 first referenced                                                                                                                                    
  symbol                                       in file                                                                                                                                         
 ---------                                 ----------------                                                                                                                                    
 VLIB_GetSizeOfCCHandle                    /opt/ezsdk/component-sources/codec_engine_3_22_01_06/examples/ti/sdo/ce/examples/codecs/face_detection/lib/face_detection.ae674<face_detection.oe674>
 VLIB_calcConnectedComponentsMaxBufferSize /opt/ezsdk/component-sources/codec_engine_3_22_01_06/examples/ti/sdo/ce/examples/codecs/face_detection/lib/face_detection.ae674<face_detection.oe674>
 VLIB_createCCMap8Bit                      /opt/ezsdk/component-sources/codec_engine_3_22_01_06/examples/ti/sdo/ce/examples/codecs/face_detection/lib/face_detection.ae674<face_detection.oe674>
 VLIB_createConnectedComponentsList        /opt/ezsdk/component-sources/codec_engine_3_22_01_06/examples/ti/sdo/ce/examples/codecs/face_detection/lib/face_detection.ae674<face_detection.oe674>
 VLIB_dilate_bin_cross                     /opt/ezsdk/component-sources/codec_engine_3_22_01_06/examples/ti/sdo/ce/examples/codecs/face_detection/lib/face_detection.ae674<face_detection.oe674>

I used a command "nm" to see VLIB i used in two platforms;

VLIB in OMAP3730 is "nm c64plus/vlib.l64p -e"
AVMBlob.obj

AVMFrame.obj

AVMInterval.obj:

but in TI8148 is

VLIB_updateUWRVarianceS16.oe674:
VLIB_weightedHistogram_1D_U16.oe674:
VLIB_weightedHistogram_1D_U8.oe674:
VLIB_weightedHistogram_nD_U16.oe674:

so,What is the difference between .oe674 and .obj files.Why the new library cann't work.

Best Regards