I am Henry Chou the senior engineer from Quadrep electronics Taiwan. We got the problesms for dcantxrx import project from starterware.
Firstly, we do the ICEV2 jummper setting as following:
J6 short
J7 open
J8 2,3 short
J10 open
But the subroutine will be loop in profile = EVMProfileGet();
However we think that the profile problems for hardware. So that we try to skip the function ,and assign the profile to 1.
But can bus driver is stiil not worked, even the UART console output is failed.
How can we do to slove the problems?
By the way, we use the same import project in IDK evaluation board. It will be the same.