This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP130SSRGZR Application guide control register level

I met the ti (SN75DP130SSRGZR  Datasheet & Application ) adjustment program can not modify the maximum word setting to BIOS firmware is write to, if there is a suggestion TI specification scratchpad support HBR2 firmware file to me

Jitter HBR2 5.4Gb/s Eye diagram mask error over  DP1.2 spec

11Lane 2 - HBR2CPAT Eye Diagram Test (TP3_EQ)72.000-715E+01 %-500 m <= VALUE <= 500 m

Thank you5483.DP_port_CN6.rar