I am looking for a DSP that fits the following needs:
4 SPI ports each is connected to 2 A/D and 1 D/A converters. I need a minimum transfer speed of 6Mbit/sec on each SPI port.
The processor should be a DSP to perform a FFT on 131000 points/s.
Can someone suggest a Processor or even better an evaluation Board that supports these features?
Thanks for your help